<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Component Inspector keeps changing pin assignments in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Component-Inspector-keeps-changing-pin-assignments/m-p/190759#M632</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to assign pins in Component&amp;nbsp; Inspector, and when I change certain ones, it will say "ERROR: Pin number differs from requested value: x" where x is a number.&amp;nbsp; Then I change the next bit assignment on the same port, and it changes other assignments by itself (and highlights everything yellow).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See screenshot for better explanation.&amp;nbsp; I have set bits 0 and 1.&amp;nbsp; If I set bit 2 to the pin the mouse pointer is on, it will change bits 0 and 1 to D7 and D0, respectively from D3 and D2.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is going on here?&amp;nbsp; I've used this before and haven't had this problem until now.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is CW 10.1 for MCF52259.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 17 Dec 2011 01:59:42 GMT</pubDate>
    <dc:creator>jrmymllr</dc:creator>
    <dc:date>2011-12-17T01:59:42Z</dc:date>
    <item>
      <title>Component Inspector keeps changing pin assignments</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Component-Inspector-keeps-changing-pin-assignments/m-p/190759#M632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to assign pins in Component&amp;nbsp; Inspector, and when I change certain ones, it will say "ERROR: Pin number differs from requested value: x" where x is a number.&amp;nbsp; Then I change the next bit assignment on the same port, and it changes other assignments by itself (and highlights everything yellow).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See screenshot for better explanation.&amp;nbsp; I have set bits 0 and 1.&amp;nbsp; If I set bit 2 to the pin the mouse pointer is on, it will change bits 0 and 1 to D7 and D0, respectively from D3 and D2.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is going on here?&amp;nbsp; I've used this before and haven't had this problem until now.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is CW 10.1 for MCF52259.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Dec 2011 01:59:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Component-Inspector-keeps-changing-pin-assignments/m-p/190759#M632</guid>
      <dc:creator>jrmymllr</dc:creator>
      <dc:date>2011-12-17T01:59:42Z</dc:date>
    </item>
    <item>
      <title>Re: Component Inspector keeps changing pin assignments</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Component-Inspector-keeps-changing-pin-assignments/m-p/190760#M633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;there could be 2 problems.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#1&lt;/P&gt;&lt;P&gt;All the bits/pins must belong to &lt;U&gt;the same port&lt;/U&gt; and must be dealt with &lt;U&gt;contiguous&lt;/U&gt;. For example, Port 0/Pins 0, 1, 2, 3 is correct whereas Port 0/Pins 0, 1, 3, 4 is not correct because the pins are not fully contiguous (unallocated pin 2 constitutes a gap between pin 1 and pin 3. For more details please see ttached screenshot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#2&lt;/P&gt;&lt;P&gt;There could also problem in UI. So please close and open the project where is the problem and try to select the pins according to instructions in point 1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Vojtech Filip&lt;BR /&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2011 16:59:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Component-Inspector-keeps-changing-pin-assignments/m-p/190760#M633</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2011-12-20T16:59:42Z</dc:date>
    </item>
  </channel>
</rss>