<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックK60 USB Module - clock requirement</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/K60-USB-Module-clock-requirement/m-p/190630#M629</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've done some searching in the forums and the help archives, but have not been able to confirm whether a 48MHz (or higher) clock is required to use the K60 USB module.&lt;BR /&gt;&lt;BR /&gt;Currently I plan on using an 8MHz crystal for the system clock (EXTAL input on the K60), can I use this to internally generate the 48MHz required for USB?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Aug 2012 23:08:34 GMT</pubDate>
    <dc:creator>rc</dc:creator>
    <dc:date>2012-08-21T23:08:34Z</dc:date>
    <item>
      <title>K60 USB Module - clock requirement</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/K60-USB-Module-clock-requirement/m-p/190630#M629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've done some searching in the forums and the help archives, but have not been able to confirm whether a 48MHz (or higher) clock is required to use the K60 USB module.&lt;BR /&gt;&lt;BR /&gt;Currently I plan on using an 8MHz crystal for the system clock (EXTAL input on the K60), can I use this to internally generate the 48MHz required for USB?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Aug 2012 23:08:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/K60-USB-Module-clock-requirement/m-p/190630#M629</guid>
      <dc:creator>rc</dc:creator>
      <dc:date>2012-08-21T23:08:34Z</dc:date>
    </item>
    <item>
      <title>Re: K60 USB Module - clock requirement</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/K60-USB-Module-clock-requirement/m-p/190631#M630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; USB FS module requires 48 MHz clock. See chapter 5.7.7 USB FS OTG Controller clocking in the reference manual (or attached picture).&lt;/P&gt;&lt;P&gt;One possible clock setting of the CPU component is shown in attached screenshot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;MVa&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Aug 2012 21:02:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/K60-USB-Module-clock-requirement/m-p/190631#M630</guid>
      <dc:creator>MVa</dc:creator>
      <dc:date>2012-08-22T21:02:07Z</dc:date>
    </item>
    <item>
      <title>Re: K60 USB Module - clock requirement</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/K60-USB-Module-clock-requirement/m-p/190632#M631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Aug 2012 03:57:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/K60-USB-Module-clock-requirement/m-p/190632#M631</guid>
      <dc:creator>rcallagh</dc:creator>
      <dc:date>2012-08-23T03:57:02Z</dc:date>
    </item>
  </channel>
</rss>