<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCXA153 i2c timeout in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/MCXA153-i2c-timeout/m-p/2299410#M6022</link>
    <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I am currently developing a project based on the MCXA153VLH microprocessor, that use the I2C peripheral.&lt;/P&gt;&lt;P&gt;Using your 'lpi2c_interrupt_b2b_transfer_master' example as a reference, I have successfully managed to read from and write to a 24C02 EEPROM.&lt;/P&gt;&lt;P&gt;I would now like to implement a timeout mechanism to prevent the process from stalling or hanging if a communication line issues occurs. Could you provide a guideline or best practices for implementing this type of control within the LPI2C driver framework?&lt;/P&gt;&lt;P&gt;Thank you very much for your help and cooperation.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
    <pubDate>Fri, 23 Jan 2026 18:48:39 GMT</pubDate>
    <dc:creator>_Ferrari_</dc:creator>
    <dc:date>2026-01-23T18:48:39Z</dc:date>
    <item>
      <title>MCXA153 i2c timeout</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/MCXA153-i2c-timeout/m-p/2299410#M6022</link>
      <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I am currently developing a project based on the MCXA153VLH microprocessor, that use the I2C peripheral.&lt;/P&gt;&lt;P&gt;Using your 'lpi2c_interrupt_b2b_transfer_master' example as a reference, I have successfully managed to read from and write to a 24C02 EEPROM.&lt;/P&gt;&lt;P&gt;I would now like to implement a timeout mechanism to prevent the process from stalling or hanging if a communication line issues occurs. Could you provide a guideline or best practices for implementing this type of control within the LPI2C driver framework?&lt;/P&gt;&lt;P&gt;Thank you very much for your help and cooperation.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jan 2026 18:48:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/MCXA153-i2c-timeout/m-p/2299410#M6022</guid>
      <dc:creator>_Ferrari_</dc:creator>
      <dc:date>2026-01-23T18:48:39Z</dc:date>
    </item>
    <item>
      <title>Re: MCXA153 i2c timeout</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/MCXA153-i2c-timeout/m-p/2300474#M6023</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202847"&gt;@_Ferrari_&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV&gt;
&lt;P&gt;You can insert the &lt;CODE&gt;MSR-&amp;gt;PLTF&lt;/CODE&gt; checking logic into the &lt;CODE&gt;LPI2C_MasterTransferNonBlocking()&lt;/CODE&gt; function of the I2C driver to detect the pin-low timeout condition.&lt;/P&gt;
&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_1-1769423981030.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/374237i4DF6AC9E9B81CC18/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_1-1769423981030.png" alt="Alice_Yang_1-1769423981030.png" /&gt;&lt;/span&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Mon, 26 Jan 2026 10:39:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/MCXA153-i2c-timeout/m-p/2300474#M6023</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2026-01-26T10:39:52Z</dc:date>
    </item>
  </channel>
</rss>