<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Allocate code in SRAMX in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Allocate-code-in-SRAMX/m-p/2189852#M5994</link>
    <description>&lt;P&gt;Dear all,&lt;BR /&gt;I'm developing a project based on the NXP MCXA153 CPU processor.&lt;BR /&gt;The project has some parts, for example interrupt routines, that need to be executed as quickly as possible.&lt;BR /&gt;I've read—please correct me if I'm wrong—that if the code is allocated in the processor's SRAMX, its execution is faster.&lt;BR /&gt;If this is the case, how do I allocate a part of my code (e.g., an interrupt routine) to the SRAMX RAM?&lt;BR /&gt;Is there an application note that explains the procedure in detail?&lt;/P&gt;&lt;P&gt;Thank you very much for your valuable and kind cooperation.&lt;/P&gt;</description>
    <pubDate>Tue, 21 Oct 2025 09:30:20 GMT</pubDate>
    <dc:creator>_Ferrari_</dc:creator>
    <dc:date>2025-10-21T09:30:20Z</dc:date>
    <item>
      <title>Allocate code in SRAMX</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Allocate-code-in-SRAMX/m-p/2189852#M5994</link>
      <description>&lt;P&gt;Dear all,&lt;BR /&gt;I'm developing a project based on the NXP MCXA153 CPU processor.&lt;BR /&gt;The project has some parts, for example interrupt routines, that need to be executed as quickly as possible.&lt;BR /&gt;I've read—please correct me if I'm wrong—that if the code is allocated in the processor's SRAMX, its execution is faster.&lt;BR /&gt;If this is the case, how do I allocate a part of my code (e.g., an interrupt routine) to the SRAMX RAM?&lt;BR /&gt;Is there an application note that explains the procedure in detail?&lt;/P&gt;&lt;P&gt;Thank you very much for your valuable and kind cooperation.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Oct 2025 09:30:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Allocate-code-in-SRAMX/m-p/2189852#M5994</guid>
      <dc:creator>_Ferrari_</dc:creator>
      <dc:date>2025-10-21T09:30:20Z</dc:date>
    </item>
    <item>
      <title>Re: Allocate code in SRAMX</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Allocate-code-in-SRAMX/m-p/2191097#M5995</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202847"&gt;@_Ferrari_&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I think you can refer to this article.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE-Knowledge-Base/Relocating-Code-and-Data-Using-the-MCUXpresso-IDE/ta-p/1103719" target="_blank"&gt;Relocating Code and Data Using the MCUXpresso IDE - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Thu, 23 Oct 2025 02:58:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Allocate-code-in-SRAMX/m-p/2191097#M5995</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2025-10-23T02:58:51Z</dc:date>
    </item>
  </channel>
</rss>