<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PN7642 code read protect in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/PN7642-code-read-protect/m-p/2101837#M5951</link>
    <description>&lt;P&gt;I am using the PN7642 processor and need to protect the user firmware image.&lt;/P&gt;&lt;P&gt;Based on the API, I am using "&lt;SPAN&gt;PN76_Sys_OTPConfigs_EnableCRP()&lt;/SPAN&gt;" which is returning 0x07 "PN76_STATUS_AUTH_ERROR" which is NOT one of the expected returns documented in the API.&lt;/P&gt;&lt;P&gt;Can you please provide a detailed example of the process of activating Code Read Protection on this processor?&amp;nbsp; There is little to no information beyond the actual function call documented in the API.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 21 May 2025 17:52:31 GMT</pubDate>
    <dc:creator>KB1</dc:creator>
    <dc:date>2025-05-21T17:52:31Z</dc:date>
    <item>
      <title>PN7642 code read protect</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/PN7642-code-read-protect/m-p/2101837#M5951</link>
      <description>&lt;P&gt;I am using the PN7642 processor and need to protect the user firmware image.&lt;/P&gt;&lt;P&gt;Based on the API, I am using "&lt;SPAN&gt;PN76_Sys_OTPConfigs_EnableCRP()&lt;/SPAN&gt;" which is returning 0x07 "PN76_STATUS_AUTH_ERROR" which is NOT one of the expected returns documented in the API.&lt;/P&gt;&lt;P&gt;Can you please provide a detailed example of the process of activating Code Read Protection on this processor?&amp;nbsp; There is little to no information beyond the actual function call documented in the API.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 May 2025 17:52:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/PN7642-code-read-protect/m-p/2101837#M5951</guid>
      <dc:creator>KB1</dc:creator>
      <dc:date>2025-05-21T17:52:31Z</dc:date>
    </item>
  </channel>
</rss>