<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: T4241 processor + DDR Issue : Waiting for D_INIT timeout. Memory may not work.</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/T4241-processor-DDR-Issue-Waiting-for-D-INIT-timeout-Memory-may/m-p/1849911#M5798</link>
    <description>&lt;P&gt;Dear NXP Team,&lt;/P&gt;&lt;P&gt;We have made a new observation: during this failure case, the DDR CKE pin is not toggling. Attached are the reference oscilloscope images for the same. Please let us know the dependencies of the same.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 18 Apr 2024 13:05:27 GMT</pubDate>
    <dc:creator>kumar_086</dc:creator>
    <dc:date>2024-04-18T13:05:27Z</dc:date>
    <item>
      <title>T4241 processor + DDR Issue : Waiting for D_INIT timeout. Memory may not work.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/T4241-processor-DDR-Issue-Waiting-for-D-INIT-timeout-Memory-may/m-p/1291395#M4729</link>
      <description>&lt;P&gt;Dear Processor Software Experts,&lt;/P&gt;&lt;P&gt;We have a custom-designed board with T4241 processor with DDR memory.&lt;/P&gt;&lt;P&gt;By following similar forum threads reduced the DDR clock frequency using&amp;nbsp;RCW[MEM_PLL_RAT] option,&amp;nbsp;from 8:1 to 5:1. Still the observation is same.&lt;/P&gt;&lt;P&gt;U-Boot log as follows,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U-Boot 2016.012.0+ga9b437f (Jun 11 2021 - 10:37:47 +0530)&lt;/P&gt;&lt;P&gt;CPU0: T4241, Version: 2.0, (0x82400020)&lt;BR /&gt;Core: e6500, Version: 2.0, (0x80400120)&lt;BR /&gt;Clock Configuration:&lt;BR /&gt;CPU0:1800 MHz, CPU1:1800 MHz, CPU2:1800 MHz, CPU3:1800 MHz,&lt;BR /&gt;CPU4:1800 MHz, CPU5:1800 MHz, CPU6:1800 MHz, CPU7:1800 MHz,&lt;BR /&gt;CPU8:1800 MHz, CPU9:1800 MHz, CPU10:1800 MHz, CPU11:1800 MHz,&lt;BR /&gt;CCB:600 MHz,&lt;BR /&gt;DDR:800 MHz (1600 MT/s data rate) (Asynchronous), IFC:150 MHz&lt;BR /&gt;FMAN1: 700 MHz&lt;BR /&gt;FMAN2: 600 MHz&lt;BR /&gt;QMAN: 300 MHz&lt;BR /&gt;PME: 466.667 MHz&lt;BR /&gt;L1: D-cache 32 KiB enabled&lt;BR /&gt;I-cache 32 KiB enabled&lt;BR /&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 0c080012 0e12120e 00000000 08000000&lt;BR /&gt;00000010: 04360848 30547a00 ec03f000 f9000000&lt;BR /&gt;00000020: 00080000 00000000 00000000 0003e000&lt;BR /&gt;00000030: 00000000 50000000 00000000 00000038&lt;BR /&gt;I2C: ready&lt;BR /&gt;Board: T4241, SERDES Reference Clocks:&lt;BR /&gt;SERDES1=125MHz SERDES2=125MHz&lt;BR /&gt;SERDES3=100MHz SERDES4=100MHz&lt;BR /&gt;SPI: ready&lt;BR /&gt;DRAM: Initializing DDR&lt;/P&gt;&lt;P&gt;DDR Size: 100000000&lt;/P&gt;&lt;P&gt;Waiting for D_INIT timeout. Memory may not work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please help.&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jun 2021 12:35:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/T4241-processor-DDR-Issue-Waiting-for-D-INIT-timeout-Memory-may/m-p/1291395#M4729</guid>
      <dc:creator>kumar_086</dc:creator>
      <dc:date>2021-06-11T12:35:50Z</dc:date>
    </item>
    <item>
      <title>Re: T4241 processor + DDR Issue : Waiting for D_INIT timeout. Memory may not work.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/T4241-processor-DDR-Issue-Waiting-for-D-INIT-timeout-Memory-may/m-p/1291674#M4733</link>
      <description>&lt;P&gt;You wrote:&lt;/P&gt;
&lt;P&gt;&amp;gt; reduced the DDR clock frequency using RCW[MEM_PLL_RAT] option, from 8:1 to 5:1&lt;/P&gt;
&lt;P&gt;This statement contradicts the U-Boot log:&lt;/P&gt;
&lt;P&gt;&amp;gt; DDR:800 MHz (1600 MT/s data rate) (Asynchronous), IFC:150 MHz&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1) Please doublecheck the SDRAM connection referring the AN3940 - Hardware and Layout Design Considerations for DDR3 SDRAM.&lt;/P&gt;
&lt;P&gt;2) Use CodeWarrior QCVS DDR Validation Tool to check/optimize the DDR controller settings.&lt;/P&gt;</description>
      <pubDate>Sun, 13 Jun 2021 16:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/T4241-processor-DDR-Issue-Waiting-for-D-INIT-timeout-Memory-may/m-p/1291674#M4733</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-06-13T16:46:46Z</dc:date>
    </item>
    <item>
      <title>Re: T4241 processor + DDR Issue : Waiting for D_INIT timeout. Memory may not work.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/T4241-processor-DDR-Issue-Waiting-for-D-INIT-timeout-Memory-may/m-p/1849911#M5798</link>
      <description>&lt;P&gt;Dear NXP Team,&lt;/P&gt;&lt;P&gt;We have made a new observation: during this failure case, the DDR CKE pin is not toggling. Attached are the reference oscilloscope images for the same. Please let us know the dependencies of the same.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 18 Apr 2024 13:05:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/T4241-processor-DDR-Issue-Waiting-for-D-INIT-timeout-Memory-may/m-p/1849911#M5798</guid>
      <dc:creator>kumar_086</dc:creator>
      <dc:date>2024-04-18T13:05:27Z</dc:date>
    </item>
  </channel>
</rss>