<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRTC problems running on target board</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/RTC-problems-running-on-target-board/m-p/188686#M579</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not sure which forum this should be addressed to but I'll start here. I'm running CW10.1 with MQX and PE using a Kinetis k60 processor. I have run programs on the twrk60n512 board just fine but now have my own target board which still uses the k60 processor. I created new bsp and psp projects which have been built. I am trying to run on the new board but am running into problems with what seems to be an RTC issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I include an RTC component using PE, then program gets as far as the routine _pe_initialize_hardware in the cpu.c file. As soon as the RTC is enabled in the statement: SIM_SCGC6 |= 0x20000000, the program goes to the kernel interrupt handler.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I don't include an RTC component in the bsp using PE, then the program makes it to line 111 in the _rtc_init routine in the file krtc.c before ending up in the kernel interrupt routine. If the program is allowed to continue from the interrupt &amp;nbsp;and then paused, the program is found&amp;nbsp;in the _pend_svc routine of the dispatch.s file in the section with the label&amp;nbsp;"no_one_to_run".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any suggestions as to how I can resolve this issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Dec 2011 08:00:05 GMT</pubDate>
    <dc:creator>ERussell</dc:creator>
    <dc:date>2011-12-08T08:00:05Z</dc:date>
    <item>
      <title>RTC problems running on target board</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/RTC-problems-running-on-target-board/m-p/188686#M579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not sure which forum this should be addressed to but I'll start here. I'm running CW10.1 with MQX and PE using a Kinetis k60 processor. I have run programs on the twrk60n512 board just fine but now have my own target board which still uses the k60 processor. I created new bsp and psp projects which have been built. I am trying to run on the new board but am running into problems with what seems to be an RTC issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I include an RTC component using PE, then program gets as far as the routine _pe_initialize_hardware in the cpu.c file. As soon as the RTC is enabled in the statement: SIM_SCGC6 |= 0x20000000, the program goes to the kernel interrupt handler.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I don't include an RTC component in the bsp using PE, then the program makes it to line 111 in the _rtc_init routine in the file krtc.c before ending up in the kernel interrupt routine. If the program is allowed to continue from the interrupt &amp;nbsp;and then paused, the program is found&amp;nbsp;in the _pend_svc routine of the dispatch.s file in the section with the label&amp;nbsp;"no_one_to_run".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any suggestions as to how I can resolve this issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2011 08:00:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/RTC-problems-running-on-target-board/m-p/188686#M579</guid>
      <dc:creator>ERussell</dc:creator>
      <dc:date>2011-12-08T08:00:05Z</dc:date>
    </item>
    <item>
      <title>Re: RTC problems running on target board</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/RTC-problems-running-on-target-board/m-p/188687#M580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This has been solved. I neglected to apply power to the VBAT pin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2011 06:54:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/RTC-problems-running-on-target-board/m-p/188687#M580</guid>
      <dc:creator>ERussell</dc:creator>
      <dc:date>2011-12-09T06:54:01Z</dc:date>
    </item>
  </channel>
</rss>