<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: Question about the operation when using imxvideoconvert_g2d with gstreamer.</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Question-about-the-operation-when-using-imxvideoconvert-g2d-with/m-p/1700986#M5688</link>
    <description>&lt;P&gt;try to use waylandsink instead appsink&lt;/P&gt;</description>
    <pubDate>Tue, 08 Aug 2023 09:23:50 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2023-08-08T09:23:50Z</dc:date>
    <item>
      <title>Question about the operation when using imxvideoconvert_g2d with gstreamer.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Question-about-the-operation-when-using-imxvideoconvert-g2d-with/m-p/1700579#M5687</link>
      <description>&lt;P&gt;I am conducting tests with the following commands in gstreamer.&lt;BR /&gt;However, when attempting to output from imxvideoconvert_g2d to appsink, the operation comes to a halt.&lt;BR /&gt;What could be the potential causes of this issue?&lt;/P&gt;&lt;P&gt;gst-launch-1.0 v4l2src device=/dev/video1 ! imxvideoconvert_g2d ! autovideosink&lt;BR /&gt;OK: Functions correctly.&lt;/P&gt;&lt;P&gt;gst-launch-1.0 v4l2src device=/dev/video1 ! videoconvert ! appsink name=sink&lt;BR /&gt;OK: Functions correctly.&lt;/P&gt;&lt;P&gt;gst-launch-1.0 v4l2src device=/dev/video1 ! imxvideoconvert_g2d ! appsink name=sink&lt;BR /&gt;NG: The operation comes to a halt.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;root@imx8mp-lpddr4-evk:~# GST_DEBUG=2 gst-launch-1.0 v4l2src device=/dev/video1 ! imxvideoconvert_g2d ! appsink name=sink&lt;BR /&gt;Setting pipeline to PAUSED ...&lt;BR /&gt;Pipeline is live and does not need PREROLL ...&lt;BR /&gt;Pipeline is PREROLLED ...&lt;BR /&gt;Setting pipeline to PLAYING ...&lt;BR /&gt;0:00:00.255372500 696 0xaaaae21c7460 WARN v4l2 gstv4l2object.c:4623:gst_v4l2_object_probe_caps:&amp;lt;v4l2src0:src&amp;gt; Failed to probe pixel aspect ratio with VIDIOC_CROPCAP: Invalid argument&lt;BR /&gt;New clock: GstSystemClock&lt;BR /&gt;[ 1054.652977] bypass csc&lt;BR /&gt;[ 1054.655368] input fmt YUV4&lt;BR /&gt;[ 1054.658074] output fmt YUYV&lt;BR /&gt;Redistribute latency...&lt;BR /&gt;0:00:00.909568750 696 0xaaaae21c7460 WARN v4l2src gstv4l2src.c:1123:gst_v4l2src_create:&amp;lt;v4l2src0&amp;gt; lost frames detected: count = 1 - ts: 0:00:00.631526250&lt;BR /&gt;0:00:00.6 / 99:99:99.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CPU:i.MX8MP&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Aug 2023 01:11:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Question-about-the-operation-when-using-imxvideoconvert-g2d-with/m-p/1700579#M5687</guid>
      <dc:creator>kuri</dc:creator>
      <dc:date>2023-08-08T01:11:40Z</dc:date>
    </item>
    <item>
      <title>Re: Question about the operation when using imxvideoconvert_g2d with gstreamer.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Question-about-the-operation-when-using-imxvideoconvert-g2d-with/m-p/1700986#M5688</link>
      <description>&lt;P&gt;try to use waylandsink instead appsink&lt;/P&gt;</description>
      <pubDate>Tue, 08 Aug 2023 09:23:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Question-about-the-operation-when-using-imxvideoconvert-g2d-with/m-p/1700986#M5688</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-08-08T09:23:50Z</dc:date>
    </item>
  </channel>
</rss>