<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: i.Mx7D Power management Issue</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/i-Mx7D-Power-management-Issue/m-p/1657110#M5591</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Which kernel version are you working with?&lt;BR /&gt;Also, if wake up trough WiFi interrupt is working we can discard a hardware issue but just to be sure could you check with an oscilloscope when attempting wakeup from sensor interrupt?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Wed, 24 May 2023 22:37:27 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2023-05-24T22:37:27Z</dc:date>
    <item>
      <title>i.Mx7D Power management Issue</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/i-Mx7D-Power-management-Issue/m-p/1655416#M5584</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; We are using i.Mx7D for one of our custom project. We are trying to achieve the power management. We have 2 wakeup source. One is PIR interrupt (GPIO2_25) and another is WIFI interrupt (GPIO2_IO0).&lt;/P&gt;&lt;P&gt;We have configured both the interrupt as a wakeupsource from dts file. But we are observing "timeout waiting for hardware interrupt." error after system resumes from suspend. I have followed the below scenario&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Put the system into sleep using "echo mem &amp;gt; /sys/power/state" command.&lt;/P&gt;&lt;P&gt;2. Wakeup the system from wifi interrupt.&amp;nbsp; &amp;nbsp;----&amp;gt; No issue&lt;/P&gt;&lt;P&gt;3. Put the system into sleep&lt;/P&gt;&lt;P&gt;4. Wakeup the system using PIR ( sensor) interrupt. ---&amp;gt;observed&amp;nbsp;sdhci dump logs in the dmesg and system becomes unstable.&lt;/P&gt;&lt;P&gt;We are using Broadcom chipset for wifi.&lt;/P&gt;&lt;P&gt;I have attached my logs.&lt;/P&gt;&lt;P&gt;Please help me to resolve this issue&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 May 2023 07:22:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/i-Mx7D-Power-management-Issue/m-p/1655416#M5584</guid>
      <dc:creator>sharmilad</dc:creator>
      <dc:date>2023-05-23T07:22:49Z</dc:date>
    </item>
    <item>
      <title>Re: i.Mx7D Power management Issue</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/i-Mx7D-Power-management-Issue/m-p/1657110#M5591</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Which kernel version are you working with?&lt;BR /&gt;Also, if wake up trough WiFi interrupt is working we can discard a hardware issue but just to be sure could you check with an oscilloscope when attempting wakeup from sensor interrupt?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 24 May 2023 22:37:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/i-Mx7D-Power-management-Issue/m-p/1657110#M5591</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2023-05-24T22:37:27Z</dc:date>
    </item>
    <item>
      <title>Re: i.Mx7D Power management Issue</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/i-Mx7D-Power-management-Issue/m-p/1676075#M5648</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Now I am successfully able to put the device into suspend mode and wakeup from gpio interrupt. My next concern is current consumption. In suspend mode my device is not reducing much current . And I could see pm-imx7.c and suspend-imx7.S file is not present in my arch/arm/mach-imx folder. Does these files are required for power management (suspend mode )? I am using kernel 5.10 version.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 13:41:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/i-Mx7D-Power-management-Issue/m-p/1676075#M5648</guid>
      <dc:creator>sharmilad</dc:creator>
      <dc:date>2023-06-26T13:41:37Z</dc:date>
    </item>
    <item>
      <title>Re: i.Mx7D Power management Issue</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/i-Mx7D-Power-management-Issue/m-p/1677200#M5656</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Glad to hear that you were successful with that, regarding consumption it would be difficult to say if its ok or not if I do not see the values for reference.&lt;BR /&gt;&lt;BR /&gt;But you may take as reference based in the measurement we did back in the days for our EVK (AN5383), for “Suspend-To-RAM” in the Linux BSP. This is the lowest possible power state where the external supplies are still on.&lt;BR /&gt;&lt;BR /&gt;Chapter 4.1.1 Deep-sleep mode (DSM)&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AldoG_0-1687890780350.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/229685iE84BF8048DB4E79E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="AldoG_0-1687890780350.png" alt="AldoG_0-1687890780350.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;BR /&gt;Also, please refer to this same App note chapter 5 Reducing Power Consumption for optimization on low power mode.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5383.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5383.pdf&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jun 2023 18:33:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/i-Mx7D-Power-management-Issue/m-p/1677200#M5656</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2023-06-27T18:33:50Z</dc:date>
    </item>
  </channel>
</rss>