<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How put in service WWAN0 interface in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/How-put-in-service-WWAN0-interface/m-p/1640714#M5539</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm working with i.mx8 and Quectel EG21 module (Yocto based) and i try to enabling wwan0 interface to connect the device with network LTE operator&lt;/P&gt;&lt;P&gt;I've update the kernel adding "qmi_wwan_q.c" file dilivered from Quectel and activate the driver via menuconfig.&lt;/P&gt;&lt;P&gt;When, from shell, I bring up the wwan0 interface i see :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;wwan0: flags=193&amp;lt;UP,RUNNING,NOARP&amp;gt; mtu 1500&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;inet6 fe80::28b5:d6ff:fe76:689 prefixlen 64 scopeid 0x20&amp;lt;link&amp;gt;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;ether 2a:b5:d6:76:06:89 txqueuelen 1000 (Ethernet)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;RX packets 0 bytes 0 (0.0 B)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;RX errors 0 dropped 0 overruns 0 frame 0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;TX packets 10 bytes 560 (560.0 B)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;where the ip address is the default ipv6 address. So I need to set the parameters so to connect with network and I image something like wpa_supplicant for wifi connection&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Someone can help me?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 02 May 2023 15:01:34 GMT</pubDate>
    <dc:creator>Ratataplam</dc:creator>
    <dc:date>2023-05-02T15:01:34Z</dc:date>
    <item>
      <title>How put in service WWAN0 interface</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-put-in-service-WWAN0-interface/m-p/1640714#M5539</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm working with i.mx8 and Quectel EG21 module (Yocto based) and i try to enabling wwan0 interface to connect the device with network LTE operator&lt;/P&gt;&lt;P&gt;I've update the kernel adding "qmi_wwan_q.c" file dilivered from Quectel and activate the driver via menuconfig.&lt;/P&gt;&lt;P&gt;When, from shell, I bring up the wwan0 interface i see :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;wwan0: flags=193&amp;lt;UP,RUNNING,NOARP&amp;gt; mtu 1500&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;inet6 fe80::28b5:d6ff:fe76:689 prefixlen 64 scopeid 0x20&amp;lt;link&amp;gt;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;ether 2a:b5:d6:76:06:89 txqueuelen 1000 (Ethernet)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;RX packets 0 bytes 0 (0.0 B)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;RX errors 0 dropped 0 overruns 0 frame 0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;TX packets 10 bytes 560 (560.0 B)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;where the ip address is the default ipv6 address. So I need to set the parameters so to connect with network and I image something like wpa_supplicant for wifi connection&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Someone can help me?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 02 May 2023 15:01:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-put-in-service-WWAN0-interface/m-p/1640714#M5539</guid>
      <dc:creator>Ratataplam</dc:creator>
      <dc:date>2023-05-02T15:01:34Z</dc:date>
    </item>
  </channel>
</rss>