<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: EQOS mac (imx-dwmac driver) freezes the system when bridge is configured</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/EQOS-mac-imx-dwmac-driver-freezes-the-system-when-bridge-is/m-p/1619941#M5508</link>
    <description>&lt;P&gt;I am having a similar issue. Did you manage to resolve it?&lt;/P&gt;</description>
    <pubDate>Wed, 22 Mar 2023 15:21:57 GMT</pubDate>
    <dc:creator>markusm</dc:creator>
    <dc:date>2023-03-22T15:21:57Z</dc:date>
    <item>
      <title>EQOS mac (imx-dwmac driver) freezes the system when bridge is configured</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/EQOS-mac-imx-dwmac-driver-freezes-the-system-when-bridge-is/m-p/1600448#M5475</link>
      <description>&lt;P&gt;I'm working on two different boards with i.MX8MP:&lt;/P&gt;&lt;P&gt;1) Board A uses a DP83867 PHY&lt;/P&gt;&lt;P&gt;2) Board B uses an Atheros AR803x PHY&lt;/P&gt;&lt;P&gt;Both works out of the box in a default setup. However, when I try to configure a bridge and assign the eqos interface (eth1) to the bridge, the whole system freezes (no kernel crash messages, nothing, just freezes...).&lt;/P&gt;&lt;P&gt;The problem was observed with two different BSPs and different kernel versions: 5.10. 5.15 and 6.2&lt;/P&gt;&lt;P&gt;Steps to reproduce it's pretty simple, just try to configure a bridge and assign eth1 to it. During the startup, when interface is being configured, the system freezes.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Feb 2023 11:39:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/EQOS-mac-imx-dwmac-driver-freezes-the-system-when-bridge-is/m-p/1600448#M5475</guid>
      <dc:creator>RenePinto</dc:creator>
      <dc:date>2023-02-16T11:39:25Z</dc:date>
    </item>
    <item>
      <title>Re: EQOS mac (imx-dwmac driver) freezes the system when bridge is configured</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/EQOS-mac-imx-dwmac-driver-freezes-the-system-when-bridge-is/m-p/1619941#M5508</link>
      <description>&lt;P&gt;I am having a similar issue. Did you manage to resolve it?&lt;/P&gt;</description>
      <pubDate>Wed, 22 Mar 2023 15:21:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/EQOS-mac-imx-dwmac-driver-freezes-the-system-when-bridge-is/m-p/1619941#M5508</guid>
      <dc:creator>markusm</dc:creator>
      <dc:date>2023-03-22T15:21:57Z</dc:date>
    </item>
    <item>
      <title>Re: EQOS mac (imx-dwmac driver) freezes the system when bridge is configured</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/EQOS-mac-imx-dwmac-driver-freezes-the-system-when-bridge-is/m-p/1619960#M5509</link>
      <description>&lt;P&gt;Yes&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/33371"&gt;@markusm&lt;/a&gt; ,my workaround was to let clocks enabled in &lt;SPAN class=""&gt;stmmac_dvr_probe&lt;/SPAN&gt;(). You can take a look here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/lf-edge/eve/pull/3085/commits/b417dacaa68de132d85171d5aa88e6c59fa76b03#diff-ce01c8460fa872fe79f3bd7b9e80e809ec7db3fd6ba4e6d3b990ae2305b5cd6c" target="_blank"&gt;https://github.com/lf-edge/eve/pull/3085/commits/b417dacaa68de132d85171d5aa88e6c59fa76b03#diff-ce01c8460fa872fe79f3bd7b9e80e809ec7db3fd6ba4e6d3b990ae2305b5cd6c&lt;/A&gt;&lt;/P&gt;&lt;P&gt;And to make bridge work properly I also applied this patch (took from this forum):&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/lf-edge/eve/pull/3085/commits/b417dacaa68de132d85171d5aa88e6c59fa76b03#diff-122b226802028bfbac4fc63f9ee3cf6ab843e54b458a6e7e1713b047bfffccdb" target="_blank" rel="noopener"&gt;https://github.com/lf-edge/eve/pull/3085/commits/b417dacaa68de132d85171d5aa88e6c59fa76b03#diff-122b226802028bfbac4fc63f9ee3cf6ab843e54b458a6e7e1713b047bfffccdb&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 22 Mar 2023 15:42:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/EQOS-mac-imx-dwmac-driver-freezes-the-system-when-bridge-is/m-p/1619960#M5509</guid>
      <dc:creator>RenePinto</dc:creator>
      <dc:date>2023-03-22T15:42:09Z</dc:date>
    </item>
  </channel>
</rss>