<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 Re: lpc55xx vbus disable</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/lpc55xx-vbus-disable/m-p/1575794#M5377</link>
    <description>&lt;P&gt;Hi&amp;nbsp;_Ferrari_&amp;nbsp;&lt;/P&gt;
&lt;P&gt;When USB as device,&amp;nbsp;&lt;SPAN&gt;USB device gets the 5V from the host via VBUS.&amp;nbsp; USB device judges whether VBUS has power to determine whether USB is plugged in. So we recomend user not disable VBUS to gurantee USB working normally.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;If you don't care if there is a disconnect event or not, you can set FORCE_ VBUS&amp;nbsp; bit to 1. It means VBUS is always connected.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;They don't need to connect VBUS pin from the connector to our USB_VBUS pin physically and the voltage level of VBUS won't matter. Thus I can't gurantee USB working stable. This is not our recommended design.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a nice day,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 30 Dec 2022 08:45:05 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2022-12-30T08:45:05Z</dc:date>
    <item>
      <title>lpc55xx vbus disable</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/lpc55xx-vbus-disable/m-p/1575603#M5376</link>
      <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;Is there any possibility to disable VBUS signal in the USB0 peripheral of LPC5526 processor ?&lt;/P&gt;&lt;P&gt;Unfortunately I have all pins busy so I'm asking if there is a possibility to disable the VBUS signal of USB0 peripheral and try to simulate USB connection in other way&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you very much for your help amnd cooperation&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Dec 2022 17:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/lpc55xx-vbus-disable/m-p/1575603#M5376</guid>
      <dc:creator>_Ferrari_</dc:creator>
      <dc:date>2022-12-29T17:20:11Z</dc:date>
    </item>
    <item>
      <title>Re: lpc55xx vbus disable</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/lpc55xx-vbus-disable/m-p/1575794#M5377</link>
      <description>&lt;P&gt;Hi&amp;nbsp;_Ferrari_&amp;nbsp;&lt;/P&gt;
&lt;P&gt;When USB as device,&amp;nbsp;&lt;SPAN&gt;USB device gets the 5V from the host via VBUS.&amp;nbsp; USB device judges whether VBUS has power to determine whether USB is plugged in. So we recomend user not disable VBUS to gurantee USB working normally.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;If you don't care if there is a disconnect event or not, you can set FORCE_ VBUS&amp;nbsp; bit to 1. It means VBUS is always connected.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;They don't need to connect VBUS pin from the connector to our USB_VBUS pin physically and the voltage level of VBUS won't matter. Thus I can't gurantee USB working stable. This is not our recommended design.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a nice day,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Dec 2022 08:45:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/lpc55xx-vbus-disable/m-p/1575794#M5377</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-12-30T08:45:05Z</dc:date>
    </item>
    <item>
      <title>Re: lpc55xx vbus disable</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/lpc55xx-vbus-disable/m-p/1575800#M5378</link>
      <description>&lt;P&gt;Ok, I understand,&lt;/P&gt;&lt;P&gt;Thank you very much and happy new year!&lt;/P&gt;</description>
      <pubDate>Fri, 30 Dec 2022 08:38:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/lpc55xx-vbus-disable/m-p/1575800#M5378</guid>
      <dc:creator>_Ferrari_</dc:creator>
      <dc:date>2022-12-30T08:38:06Z</dc:date>
    </item>
    <item>
      <title>Re: lpc55xx vbus disable</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/lpc55xx-vbus-disable/m-p/2078420#M5942</link>
      <description>&lt;P&gt;where to find the&amp;nbsp;&lt;SPAN&gt;FORCE_ VBUS?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Apr 2025 14:22:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/lpc55xx-vbus-disable/m-p/2078420#M5942</guid>
      <dc:creator>madhubanti</dc:creator>
      <dc:date>2025-04-10T14:22:12Z</dc:date>
    </item>
  </channel>
</rss>