<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: configure GPIO as input in imx8mp in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/configure-GPIO-as-input-in-imx8mp/m-p/1569350#M5360</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204890"&gt;@DEEPIKA19&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;In the case of the &lt;EM&gt;GPIO5_IO25&lt;/EM&gt;, it should be mentioned that when a GPIO is exported in the &lt;EM&gt;sysfs,&amp;nbsp;&lt;/EM&gt;by default, the direction of the GPIO is set as &lt;EM&gt;"input,"&lt;/EM&gt; and the value is set to &lt;EM&gt;"zero."&amp;nbsp;&lt;/EM&gt;The processor itself drives the voltage level of that particular GPIO.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For the &lt;EM&gt;GPIO5_IO05&lt;/EM&gt;, please confirm the voltage at the processor side of the&amp;nbsp;&lt;EM&gt;GPIO5_IO05&lt;/EM&gt;&amp;nbsp;before and after exporting the GPIO.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;And also, please confirm if the GPIO5_IO05 is not used in the device tree by any other peripheral.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit.&lt;/P&gt;</description>
    <pubDate>Wed, 14 Dec 2022 04:19:37 GMT</pubDate>
    <dc:creator>Dhruvit</dc:creator>
    <dc:date>2022-12-14T04:19:37Z</dc:date>
    <item>
      <title>configure GPIO as input in imx8mp</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/configure-GPIO-as-input-in-imx8mp/m-p/1568771#M5359</link>
      <description>&lt;P&gt;Hi team&lt;/P&gt;&lt;P&gt;I would like to use the GPIO5_IO25 as a input pin in our design. By default when exported from sysfs I am getting the following value.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:root@root:/sys/class/gpio/gpio153" target="_blank"&gt;root@root:/sys/class/gpio/gpio153#&lt;/A&gt;&amp;nbsp;cat direction&lt;/P&gt;&lt;P&gt;in&lt;/P&gt;&lt;P&gt;root@root:/sys/class/gpio/gpio153# cat value&lt;/P&gt;&lt;P&gt;0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The GPIO5_IO05 is connected to a 10k pullup but the value is 0. Please could someone suggest me on how to debug this. Should any dts changes be added for this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Deepika&lt;/P&gt;</description>
      <pubDate>Tue, 13 Dec 2022 05:45:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/configure-GPIO-as-input-in-imx8mp/m-p/1568771#M5359</guid>
      <dc:creator>DEEPIKA19</dc:creator>
      <dc:date>2022-12-13T05:45:19Z</dc:date>
    </item>
    <item>
      <title>Re: configure GPIO as input in imx8mp</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/configure-GPIO-as-input-in-imx8mp/m-p/1569350#M5360</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204890"&gt;@DEEPIKA19&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;In the case of the &lt;EM&gt;GPIO5_IO25&lt;/EM&gt;, it should be mentioned that when a GPIO is exported in the &lt;EM&gt;sysfs,&amp;nbsp;&lt;/EM&gt;by default, the direction of the GPIO is set as &lt;EM&gt;"input,"&lt;/EM&gt; and the value is set to &lt;EM&gt;"zero."&amp;nbsp;&lt;/EM&gt;The processor itself drives the voltage level of that particular GPIO.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For the &lt;EM&gt;GPIO5_IO05&lt;/EM&gt;, please confirm the voltage at the processor side of the&amp;nbsp;&lt;EM&gt;GPIO5_IO05&lt;/EM&gt;&amp;nbsp;before and after exporting the GPIO.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;And also, please confirm if the GPIO5_IO05 is not used in the device tree by any other peripheral.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Dec 2022 04:19:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/configure-GPIO-as-input-in-imx8mp/m-p/1569350#M5360</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2022-12-14T04:19:37Z</dc:date>
    </item>
    <item>
      <title>Re: configure GPIO as input in imx8mp</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/configure-GPIO-as-input-in-imx8mp/m-p/1575112#M5371</link>
      <description>&lt;P&gt;hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Deepika&lt;/P&gt;</description>
      <pubDate>Wed, 28 Dec 2022 07:39:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/configure-GPIO-as-input-in-imx8mp/m-p/1575112#M5371</guid>
      <dc:creator>DEEPIKA19</dc:creator>
      <dc:date>2022-12-28T07:39:05Z</dc:date>
    </item>
    <item>
      <title>Re: configure GPIO as input in imx8mp</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/configure-GPIO-as-input-in-imx8mp/m-p/1578420#M5387</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204890"&gt;@DEEPIKA19&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If this issue is resolved, then Can I mark this case to close state?&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;
&lt;P&gt;Dhruvit Vasavda&lt;/P&gt;</description>
      <pubDate>Fri, 06 Jan 2023 07:54:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/configure-GPIO-as-input-in-imx8mp/m-p/1578420#M5387</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-01-06T07:54:34Z</dc:date>
    </item>
    <item>
      <title>Re: configure GPIO as input in imx8mp</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/configure-GPIO-as-input-in-imx8mp/m-p/1579048#M5388</link>
      <description>&lt;P&gt;hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;The issue is not resolved.&lt;/P&gt;&lt;P&gt;I tried to add&amp;nbsp;&lt;SPAN&gt;device_init_wakeup(&amp;amp;client-&amp;gt;dev, 1) as suggested but i am still facing the the same issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Deepika&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 09 Jan 2023 07:13:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/configure-GPIO-as-input-in-imx8mp/m-p/1579048#M5388</guid>
      <dc:creator>DEEPIKA19</dc:creator>
      <dc:date>2023-01-09T07:13:38Z</dc:date>
    </item>
    <item>
      <title>Re: configure GPIO as input in imx8mp</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/configure-GPIO-as-input-in-imx8mp/m-p/1579849#M5389</link>
      <description>&lt;P&gt;Thanks for your support&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;The issues is resolved making driver change in reference with similar touch drivers .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Deepika&lt;/P&gt;</description>
      <pubDate>Tue, 10 Jan 2023 07:40:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/configure-GPIO-as-input-in-imx8mp/m-p/1579849#M5389</guid>
      <dc:creator>DEEPIKA19</dc:creator>
      <dc:date>2023-01-10T07:40:54Z</dc:date>
    </item>
  </channel>
</rss>