<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックWhere is the low level function source code?</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Where-is-the-low-level-function-source-code/m-p/185553#M527</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like export the "Generated_code" to my existing CW project, I can't find the&lt;/P&gt;&lt;P&gt;source code of the low level functions. The compiler will fail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, in the &lt;STRONG&gt;UART3&lt;/STRONG&gt; component, there is function&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;LDD_TDeviceData* CMD_Uart3_Init(LDD_TUserData *UserDataPtr), &lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;inside this function there is low level function&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;UART_PDD_SetBaudRate(UART3_BASE_PTR, 11U); /* Set the baud rate register. */&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't find its source code, the compiler will fail on&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;Undefined : "UART_PDD_SetBaudRate"&lt;/EM&gt;&lt;/STRONG&gt;. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where is the low level source code?&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Samuel&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Nov 2012 06:19:19 GMT</pubDate>
    <dc:creator>rabbit</dc:creator>
    <dc:date>2012-11-23T06:19:19Z</dc:date>
    <item>
      <title>Where is the low level function source code?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Where-is-the-low-level-function-source-code/m-p/185553#M527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like export the "Generated_code" to my existing CW project, I can't find the&lt;/P&gt;&lt;P&gt;source code of the low level functions. The compiler will fail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, in the &lt;STRONG&gt;UART3&lt;/STRONG&gt; component, there is function&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;LDD_TDeviceData* CMD_Uart3_Init(LDD_TUserData *UserDataPtr), &lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;inside this function there is low level function&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;UART_PDD_SetBaudRate(UART3_BASE_PTR, 11U); /* Set the baud rate register. */&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't find its source code, the compiler will fail on&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;Undefined : "UART_PDD_SetBaudRate"&lt;/EM&gt;&lt;/STRONG&gt;. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where is the low level source code?&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Samuel&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Nov 2012 06:19:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Where-is-the-low-level-function-source-code/m-p/185553#M527</guid>
      <dc:creator>rabbit</dc:creator>
      <dc:date>2012-11-23T06:19:19Z</dc:date>
    </item>
    <item>
      <title>Re: Where is the low level function source code?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Where-is-the-low-level-function-source-code/m-p/185554#M528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the PDD macros are stored under the following path:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;{YOUR INSTALLATION}\MCU\ProcessorExpert\lib\Kinetis\pdd\inc\&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Details also in this thread:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="2022" data-containertype="14" data-objectid="302128" data-objecttype="1" href="https://community.nxp.com/thread/302128"&gt;Missing #include "GPIO_PDD.h" from Generated Code&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Vojtech Filip&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Nov 2012 08:28:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Where-is-the-low-level-function-source-code/m-p/185554#M528</guid>
      <dc:creator>vfilip</dc:creator>
      <dc:date>2012-11-23T08:28:51Z</dc:date>
    </item>
  </channel>
</rss>