<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: Abnormal behavior while reading VCNL4200 proximity sensor</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1511977#M5229</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Is this issue occurring in the&amp;nbsp;[i2c_polling_b2b_master] example too?&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Pavel&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 25 Aug 2022 22:35:29 GMT</pubDate>
    <dc:creator>Pavel_Hernandez</dc:creator>
    <dc:date>2022-08-25T22:35:29Z</dc:date>
    <item>
      <title>Abnormal behavior while reading VCNL4200 proximity sensor</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1510409#M5225</link>
      <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I connected the LPC55S28-EVK to the proximity sensor VCNL4200. The LPC55S28-EVK is configured as master and VCNL4200, of course, as slave.&lt;/P&gt;&lt;P&gt;I developed a simple software to read the DeviceID of the sensor: in an endless while I inserted the reading of the DeviceID&amp;nbsp; of the sensor&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt; int i =0;
 while(1) {
        i++ ;
        /* 'Dummy' NOP to allow source level single stepping of
            tight while() loop */
        __asm volatile ("nop");
        int res= readID();
        PRINTF("%3d %x\n",i,res);
    }&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;the readID funcrion is:&lt;/P&gt;&lt;PRE&gt;#define EXAMPLE_I2C_MASTER FLEXCOMM4_PERIPHERAL
#define I2C_MASTER_SLAVE_ADDR_7BIT VCNL4200_I2CADDR
#define I2C_DATA_LENGTH 2
uint8_t g_master_txBuff[I2C_DATA_LENGTH];
uint8_t g_master_rxBuff[I2C_DATA_LENGTH];

int readID() {
	int ID;
    //if (readData(VCNL4200_DeviceID_REG) != 0x1058)
    ID=readData(VCNL4200_DeviceID_REG);
	return ID;
}

uint16_t readData(uint8_t command_code) {
	uint8_t deviceAddress;
	deviceAddress=command_code;
	status_t reVal        = kStatus_Fail;
  if (kStatus_Success == I2C_MasterStart(EXAMPLE_I2C_MASTER, I2C_MASTER_SLAVE_ADDR_7BIT, kI2C_Write))
    {
        reVal = I2C_MasterWriteBlocking(EXAMPLE_I2C_MASTER, &amp;amp;deviceAddress, 1, kI2C_TransferNoStopFlag);
        if (reVal != kStatus_Success)
        {
            return -1;
        }

        reVal = I2C_MasterRepeatedStart(EXAMPLE_I2C_MASTER, I2C_MASTER_SLAVE_ADDR_7BIT, kI2C_Read);
        if (reVal != kStatus_Success)
        {
            return -1;
        }

        reVal =I2C_MasterReadBlocking(EXAMPLE_I2C_MASTER, g_master_rxBuff, I2C_DATA_LENGTH, kI2C_TransferDefaultFlag);
        if (reVal != kStatus_Success)
        {
            return -1;
        }

        reVal = I2C_MasterStop(EXAMPLE_I2C_MASTER);
        if (reVal != kStatus_Success)
        {
            return -1;
        }
    }
	return g_master_rxBuff[1]&amp;lt;&amp;lt;8 | g_master_rxBuff[0];
}&lt;/PRE&gt;&lt;P&gt;I used MCUXpresso IDE v11.5.1 [Build 7266] [2022-04-13] and the routine&amp;nbsp; readData is developed according the i2c_polling_b2b_master.c example.&lt;/P&gt;&lt;P&gt;According the datasheet of VCNL4200 VCNL4200_I2CADDR is 0x51 and VCNL4200_DeviceID_REG id 0x0E.&lt;/P&gt;&lt;P&gt;I connected the proximity sensor to the demo board as following:&lt;/P&gt;&lt;P&gt;I2C_SCL P17-1 I2C_SCL P17-1&lt;BR /&gt;I2C_SDA P17-3 I2C_SDA P17-3&lt;BR /&gt;GND P17-7 GND P17-7&lt;/P&gt;&lt;P&gt;and I used P16-8 (3.3V) as power supply of the proximity sensor.&lt;/P&gt;&lt;P&gt;I compiled the software and I debugged it but the data displayed on the console is:&lt;/P&gt;&lt;P&gt;Hello World&lt;BR /&gt;1 ffff&lt;BR /&gt;2 1058&lt;BR /&gt;3 ffff&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;only three readings are made and only the second one is correct.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;After the third reading the program hangs-up in the routine I2C_PendingStatusWait.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Did you have a similar problem ?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;How did you fix it ?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Thank you very much for your help and cooperation.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Best regards.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Aug 2022 21:13:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1510409#M5225</guid>
      <dc:creator>_Ferrari_</dc:creator>
      <dc:date>2022-08-23T21:13:31Z</dc:date>
    </item>
    <item>
      <title>Re: Abnormal behavior while reading VCNL4200 proximity sensor</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1511977#M5229</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Is this issue occurring in the&amp;nbsp;[i2c_polling_b2b_master] example too?&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Pavel&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Aug 2022 22:35:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1511977#M5229</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-08-25T22:35:29Z</dc:date>
    </item>
    <item>
      <title>Re: Abnormal behavior while reading VCNL4200 proximity sensor</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1512399#M5230</link>
      <description>&lt;P&gt;Dear Pavel,&lt;/P&gt;&lt;P&gt;thank you for your replly.&lt;/P&gt;&lt;P&gt;You wrote:&lt;/P&gt;&lt;P&gt;&amp;gt; Is this issue occurring in the [i2c_polling_b2b_master] example too?&lt;/P&gt;&lt;P&gt;Yes, I have the same issue&lt;/P&gt;&lt;P&gt;Thank you very much for your help and cooperation&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Aug 2022 13:38:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1512399#M5230</guid>
      <dc:creator>_Ferrari_</dc:creator>
      <dc:date>2022-08-26T13:38:13Z</dc:date>
    </item>
    <item>
      <title>Re: Abnormal behavior while reading VCNL4200 proximity sensor</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1512582#M5231</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I review the code on my side and it works as expected, could you review your code, or in another case could you update the SDK and the IDE?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Fri, 26 Aug 2022 20:22:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1512582#M5231</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-08-26T20:22:09Z</dc:date>
    </item>
    <item>
      <title>Re: Abnormal behavior while reading VCNL4200 proximity sensor</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1514652#M5233</link>
      <description>&lt;P&gt;Yes, I have the same issue&lt;/P&gt;&lt;P&gt;Thank you very much for your help and cooperation&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Wed, 31 Aug 2022 13:13:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1514652#M5233</guid>
      <dc:creator>_Ferrari_</dc:creator>
      <dc:date>2022-08-31T13:13:01Z</dc:date>
    </item>
    <item>
      <title>Re: Abnormal behavior while reading VCNL4200 proximity sensor</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1517204#M5239</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I apologize for the late response, I will share with you an example that works in the LPC55s28 EVK, you can test and if this does not work maybe you have something missing in your hardware. If this does not work, Could you share the image from the logic analyzer to review the frame?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Mon, 05 Sep 2022 18:32:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1517204#M5239</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-09-05T18:32:07Z</dc:date>
    </item>
    <item>
      <title>Re: Abnormal behavior while reading VCNL4200 proximity sensor</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1522015#M5247</link>
      <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I downloaded the project that handles the on board accellerometer and it worls.&lt;/P&gt;&lt;P&gt;Unfortunately the I2C periheral can't be configured by the MCUXpresso periherals configurator.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Wed, 14 Sep 2022 13:57:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1522015#M5247</guid>
      <dc:creator>_Ferrari_</dc:creator>
      <dc:date>2022-09-14T13:57:17Z</dc:date>
    </item>
    <item>
      <title>Re: Abnormal behavior while reading VCNL4200 proximity sensor</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1522065#M5248</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;What do you need to modify in the configuration of the I2C? The image below is from the config tool.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1663168967091.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/193646i674CD593631E2E60/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_0-1663168967091.png" alt="Pavel_Hernandez_0-1663168967091.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Pavel_Hernandez_0-1663168967091.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Sep 2022 15:23:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Abnormal-behavior-while-reading-VCNL4200-proximity-sensor/m-p/1522065#M5248</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-09-14T15:23:22Z</dc:date>
    </item>
  </channel>
</rss>