<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックXIP stops running after boot on custom MIMXRT1015 board</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/XIP-stops-running-after-boot-on-custom-MIMXRT1015-board/m-p/1490424#M5184</link>
    <description>&lt;P&gt;Hi, I have a custom board running just a blink example. The board is based on the MIMXRT1015 EVK. It has the same flash chip, but uses the 4A package instead of 5A. Whenever I flash the chip, I can see the flash being programmed on an oscilloscope. The link I am using says it verifies the flash correctly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Whenever the MCU boots, I can see the flash start up but immediately stops. Debugging never gets to main. When I execute the code from RAM it works correctly. Has anyone seen something like this?&lt;/P&gt;</description>
    <pubDate>Fri, 15 Jul 2022 15:12:41 GMT</pubDate>
    <dc:creator>EricBuschCDI</dc:creator>
    <dc:date>2022-07-15T15:12:41Z</dc:date>
    <item>
      <title>XIP stops running after boot on custom MIMXRT1015 board</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/XIP-stops-running-after-boot-on-custom-MIMXRT1015-board/m-p/1490424#M5184</link>
      <description>&lt;P&gt;Hi, I have a custom board running just a blink example. The board is based on the MIMXRT1015 EVK. It has the same flash chip, but uses the 4A package instead of 5A. Whenever I flash the chip, I can see the flash being programmed on an oscilloscope. The link I am using says it verifies the flash correctly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Whenever the MCU boots, I can see the flash start up but immediately stops. Debugging never gets to main. When I execute the code from RAM it works correctly. Has anyone seen something like this?&lt;/P&gt;</description>
      <pubDate>Fri, 15 Jul 2022 15:12:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/XIP-stops-running-after-boot-on-custom-MIMXRT1015-board/m-p/1490424#M5184</guid>
      <dc:creator>EricBuschCDI</dc:creator>
      <dc:date>2022-07-15T15:12:41Z</dc:date>
    </item>
  </channel>
</rss>