<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx8mq low power mode in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/imx8mq-low-power-mode/m-p/1463212#M5138</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are working imx8mq custom board and require to put processor in low power mode in order to reduce power consumption. As per AN13400 there are two low power modes, 1) Wait and Stop Mode 2) DSM. We have tried DSM mode and it reduces power consumption but also want to try&amp;nbsp;Wait and Stop Mode. So, how to put processor into this mode?&amp;nbsp;&lt;/P&gt;&lt;P&gt;NOTE: - There are some registers which needs to be configured as per AN13400 but how we can configure them?&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13400.pdf" target="_blank"&gt;AN13400.pdf (nxp.com)&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 24 May 2022 11:49:53 GMT</pubDate>
    <dc:creator>Aakash_Sharma</dc:creator>
    <dc:date>2022-05-24T11:49:53Z</dc:date>
    <item>
      <title>imx8mq low power mode</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/imx8mq-low-power-mode/m-p/1463212#M5138</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are working imx8mq custom board and require to put processor in low power mode in order to reduce power consumption. As per AN13400 there are two low power modes, 1) Wait and Stop Mode 2) DSM. We have tried DSM mode and it reduces power consumption but also want to try&amp;nbsp;Wait and Stop Mode. So, how to put processor into this mode?&amp;nbsp;&lt;/P&gt;&lt;P&gt;NOTE: - There are some registers which needs to be configured as per AN13400 but how we can configure them?&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13400.pdf" target="_blank"&gt;AN13400.pdf (nxp.com)&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 24 May 2022 11:49:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/imx8mq-low-power-mode/m-p/1463212#M5138</guid>
      <dc:creator>Aakash_Sharma</dc:creator>
      <dc:date>2022-05-24T11:49:53Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq low power mode</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/imx8mq-low-power-mode/m-p/1490560#M5185</link>
      <description>&lt;P&gt;3.2 Low-power modes on i.MX 8M This section describes the specifics of low-power modes on i.MX 8M and the difference between Suspend mode and DSM (Deep Sleep mode). 3.2.1 SoC low-power modes introduction There are two platform low-power modes, Wait and Stop, and one system low-power mode, DSM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Greeting,&lt;/P&gt;&lt;P&gt;Rachel Gomez&lt;/P&gt;</description>
      <pubDate>Sat, 16 Jul 2022 06:49:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/imx8mq-low-power-mode/m-p/1490560#M5185</guid>
      <dc:creator>RachelGomez123</dc:creator>
      <dc:date>2022-07-16T06:49:17Z</dc:date>
    </item>
  </channel>
</rss>