<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックAutomated ROM/RAM page swapping MPC/SPC 560xB</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Automated-ROM-RAM-page-swapping-MPC-SPC-560xB/m-p/1460252#M5131</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would need a solution to implement an&amp;nbsp;automated ROM/RAM page swapping during run-time.&lt;/P&gt;&lt;P&gt;By default I will keep the calibration parameters in ROM, but on a request&amp;nbsp;via a single manual cal change I would like to relocate the Read-Only cal parameters from ROM to RAM and allow calibration changes.&lt;/P&gt;&lt;P&gt;If I build the code as Position-Independent, will I be able to copy the calibration section to RAM and access the calibration parameters?&lt;/P&gt;&lt;P&gt;Compiler: Wind River Diab 5.9&lt;/P&gt;</description>
    <pubDate>Wed, 18 May 2022 19:12:55 GMT</pubDate>
    <dc:creator>DIvanov</dc:creator>
    <dc:date>2022-05-18T19:12:55Z</dc:date>
    <item>
      <title>Automated ROM/RAM page swapping MPC/SPC 560xB</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Automated-ROM-RAM-page-swapping-MPC-SPC-560xB/m-p/1460252#M5131</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would need a solution to implement an&amp;nbsp;automated ROM/RAM page swapping during run-time.&lt;/P&gt;&lt;P&gt;By default I will keep the calibration parameters in ROM, but on a request&amp;nbsp;via a single manual cal change I would like to relocate the Read-Only cal parameters from ROM to RAM and allow calibration changes.&lt;/P&gt;&lt;P&gt;If I build the code as Position-Independent, will I be able to copy the calibration section to RAM and access the calibration parameters?&lt;/P&gt;&lt;P&gt;Compiler: Wind River Diab 5.9&lt;/P&gt;</description>
      <pubDate>Wed, 18 May 2022 19:12:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Automated-ROM-RAM-page-swapping-MPC-SPC-560xB/m-p/1460252#M5131</guid>
      <dc:creator>DIvanov</dc:creator>
      <dc:date>2022-05-18T19:12:55Z</dc:date>
    </item>
    <item>
      <title>Re: Automated ROM/RAM page swapping MPC/SPC 560xB</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Automated-ROM-RAM-page-swapping-MPC-SPC-560xB/m-p/1460572#M5134</link>
      <description>&lt;P&gt;Hi Daniel,&lt;/P&gt;
&lt;P&gt;this needs to be completely managed by software because there's no hardware feature which would help with remapping. Devices with e200z0 core does not have Memory Management Unit (MMU).&lt;/P&gt;
&lt;P&gt;This can be easily done on other MPC56xx devices with other cores (different from e200z0) because those have MMU. In case of MPC57xx only MPC5777C, MPC5775E, MPC5775B have MMU. Other MPC57xx have Overlay feature for this purpose.&lt;/P&gt;
&lt;P&gt;Easiest option I can see is to use a base address to read the parameters which can be changed as needed.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 19 May 2022 05:29:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Automated-ROM-RAM-page-swapping-MPC-SPC-560xB/m-p/1460572#M5134</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-05-19T05:29:35Z</dc:date>
    </item>
  </channel>
</rss>