<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: ADC Channels</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/ADC-Channels/m-p/1423262#M5028</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;PDB module has 2 channels, each channel has 8 pretriggers, so total 16 samples can be converted sequentially upon trigger from PDB on single ADC module. Same for second PDB/ADC modules.&lt;BR /&gt;At the same time 2 channels can be converted simultaneously, one on each ADC module.&lt;BR /&gt;You can refer to below example showing usage of SDK driver to do multiple channel conversions;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-DMA-S32DS-ARM-2018-R1/ta-p/1101686" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-DMA-S32DS-ARM-2018-R1/ta-p/1101686&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Fri, 04 Mar 2022 11:14:45 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2022-03-04T11:14:45Z</dc:date>
    <item>
      <title>ADC Channels</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/ADC-Channels/m-p/1422537#M5027</link>
      <description>&lt;P&gt;I want to Monitor 12 ADC channels at a time in S32K144. There are two timers/trigger LPIT AND PDB present to configure ADC channels. What I observed is there are 4 LPIT channel and 2 PDB(number of trigger slot 1 and pre-trigger slot -8)slots present. &amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please support by suggesting solution to my below query :&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;how many channels I can use at a time( I required 12 ADC to monitor at a time)&lt;/LI&gt;&lt;LI&gt;How many LPIT and PDB channels I require to configure ADC.&lt;/LI&gt;&lt;/OL&gt;</description>
      <pubDate>Thu, 03 Mar 2022 08:46:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/ADC-Channels/m-p/1422537#M5027</guid>
      <dc:creator>Gargi2021</dc:creator>
      <dc:date>2022-03-03T08:46:24Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Channels</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/ADC-Channels/m-p/1423262#M5028</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;PDB module has 2 channels, each channel has 8 pretriggers, so total 16 samples can be converted sequentially upon trigger from PDB on single ADC module. Same for second PDB/ADC modules.&lt;BR /&gt;At the same time 2 channels can be converted simultaneously, one on each ADC module.&lt;BR /&gt;You can refer to below example showing usage of SDK driver to do multiple channel conversions;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-DMA-S32DS-ARM-2018-R1/ta-p/1101686" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-DMA-S32DS-ARM-2018-R1/ta-p/1101686&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 04 Mar 2022 11:14:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/ADC-Channels/m-p/1423262#M5028</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-03-04T11:14:45Z</dc:date>
    </item>
  </channel>
</rss>