<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: Missing Processor Expert Component Property</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Missing-Processor-Expert-Component-Property/m-p/1404400#M4966</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/13026"&gt;@ZhangJennie&lt;/a&gt;&amp;nbsp;- thanks for that, looks like I might need a CodeWarrior update, I am running CW10.2 and the&amp;nbsp;&lt;STRONG&gt;Z&lt;/STRONG&gt; device doesn't show it:&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PhilV_0-1643096607652.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/168747i958FADF641959233/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PhilV_0-1643096607652.png" alt="PhilV_0-1643096607652.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I had assumed (apparently incorrectly!) that being an older device the support would be the same. I'll try updating and see if it 'appears'.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jan 2022 07:44:13 GMT</pubDate>
    <dc:creator>PhilV</dc:creator>
    <dc:date>2022-01-25T07:44:13Z</dc:date>
    <item>
      <title>Missing Processor Expert Component Property</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Missing-Processor-Expert-Component-Property/m-p/1402710#M4957</link>
      <description>&lt;P&gt;I am configuring a project so that it can operate on both MK60DN512VMD10, and as an alternative MK60DN512&lt;STRONG&gt;Z&lt;/STRONG&gt;VMD10.&lt;/P&gt;&lt;P&gt;According to the 'About' in CodeWarrior I am using:&lt;/P&gt;&lt;P&gt;Processor Expert for MCU&lt;BR /&gt;Version 5.3.0&lt;BR /&gt;Build: b1221-0685&lt;/P&gt;&lt;P&gt;When I use the MK60DN512VMD10 cpu and configure an Init_ADC component type I am able to specify the Offset value, which when code generation is done produces the appropriate register setting:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Offset is present (and set to 4)" style="width: 538px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/168388i12D98C0CD7BDFA90/image-size/large?v=v2&amp;amp;px=999" role="button" title="AD1_ADC_Init__Offset.png" alt="Offset is present (and set to 4)" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Offset is present (and set to 4)&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Generated code:&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;LI-CODE lang="cpp"&gt;// from the comment block at the start of the file:

**              Compare function                           : Result &amp;lt; CV1
**            Offset                                       : 4
**            Voltage reference                            : Default pin pair

// then later in the Init function

  /* ADC1_OFS: ??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,OFS=4 */
  ADC1_OFS = (uint32_t)0x04UL;                  &lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, when I switch to the MK60DN512&lt;STRONG&gt;Z&lt;/STRONG&gt;VMD10 cpu the offset value is missing from the "Settings group":&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="'Z' cpu missing Offset" style="width: 534px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/168389iDA4DC3AEFB437AA9/image-size/large?v=v2&amp;amp;px=999" role="button" title="AD1_ADC_Init__Offset__missingFromZ.png" alt="'Z' cpu missing Offset" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;'Z' cpu missing Offset&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Unsurprisingly the generated code is then also missing the corresponding line from the comment block, and the actual write to the registers.&lt;/P&gt;&lt;P&gt;I have checked the reference manual for both CPUs and the register is present for both as far as I can tell.&lt;/P&gt;&lt;P&gt;Q1. Why is it missing - is this an error in the CPU definition that processor expert is using?&lt;BR /&gt;Q2. Are the CPU definitions in a form that can be updated? - I know some tools use xml files to control the editor fields; is there some way I can 'tell' Processor Expert that this register&amp;nbsp;&lt;EM&gt;does&lt;/EM&gt; exist for the 'Z' cpu?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jan 2022 14:38:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Missing-Processor-Expert-Component-Property/m-p/1402710#M4957</guid>
      <dc:creator>PhilV</dc:creator>
      <dc:date>2022-01-20T14:38:49Z</dc:date>
    </item>
    <item>
      <title>Re: Missing Processor Expert Component Property</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Missing-Processor-Expert-Component-Property/m-p/1403504#M4959</link>
      <description>&lt;P&gt;&lt;EM&gt;Processor Expert&lt;/EM&gt;&lt;SPAN&gt;&amp;nbsp;for MCU Version 5.3.0. Build: b1221-0685. When I use the MK60DN512VMD10&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;cpu&lt;/EM&gt;&lt;SPAN&gt;&amp;nbsp;and configure an Init_ADC&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;component&lt;/EM&gt;&lt;SPAN&gt;&amp;nbsp;type .&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.imessageapp.bid/" target="_self"&gt;&lt;SPAN&gt;iMessage For Android&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jan 2022 04:03:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Missing-Processor-Expert-Component-Property/m-p/1403504#M4959</guid>
      <dc:creator>Mary11</dc:creator>
      <dc:date>2022-01-24T04:03:36Z</dc:date>
    </item>
    <item>
      <title>Re: Missing Processor Expert Component Property</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Missing-Processor-Expert-Component-Property/m-p/1403807#M4963</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196071"&gt;@Mary11&lt;/a&gt;&amp;nbsp;- Not sure what you were trying say above - looks like there was a problem posting the message?&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jan 2022 07:56:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Missing-Processor-Expert-Component-Property/m-p/1403807#M4963</guid>
      <dc:creator>PhilV</dc:creator>
      <dc:date>2022-01-24T07:56:47Z</dc:date>
    </item>
    <item>
      <title>Re: Missing Processor Expert Component Property</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Missing-Processor-Expert-Component-Property/m-p/1404385#M4965</link>
      <description>&lt;P&gt;HI&amp;nbsp;PhilV&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I tested this with CW11.1, I couldn't reproduce it on&amp;nbsp;&lt;SPAN&gt;MK60DN512&lt;/SPAN&gt;&lt;STRONG&gt;Z&lt;/STRONG&gt;&lt;SPAN&gt;VMD10. See below screenshot&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhangJennie_0-1643096034600.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/168743iABE6C822333F4AD8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhangJennie_0-1643096034600.png" alt="ZhangJennie_0-1643096034600.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhangJennie_1-1643096084266.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/168744i1EC565A7B5DAADC6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhangJennie_1-1643096084266.png" alt="ZhangJennie_1-1643096084266.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Where is missing?&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jan 2022 07:35:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Missing-Processor-Expert-Component-Property/m-p/1404385#M4965</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-01-25T07:35:16Z</dc:date>
    </item>
    <item>
      <title>Re: Missing Processor Expert Component Property</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Missing-Processor-Expert-Component-Property/m-p/1404400#M4966</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/13026"&gt;@ZhangJennie&lt;/a&gt;&amp;nbsp;- thanks for that, looks like I might need a CodeWarrior update, I am running CW10.2 and the&amp;nbsp;&lt;STRONG&gt;Z&lt;/STRONG&gt; device doesn't show it:&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PhilV_0-1643096607652.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/168747i958FADF641959233/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PhilV_0-1643096607652.png" alt="PhilV_0-1643096607652.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I had assumed (apparently incorrectly!) that being an older device the support would be the same. I'll try updating and see if it 'appears'.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jan 2022 07:44:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Missing-Processor-Expert-Component-Property/m-p/1404400#M4966</guid>
      <dc:creator>PhilV</dc:creator>
      <dc:date>2022-01-25T07:44:13Z</dc:date>
    </item>
    <item>
      <title>Re: Missing Processor Expert Component Property</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Missing-Processor-Expert-Component-Property/m-p/1593770#M5447</link>
      <description>&lt;P&gt;&lt;SPAN&gt;NXP is at the center of a&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;chip supply shortage&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;that has roiled the electronics industry for more than a year, unresolved due to soaring demand for electronic goods such as personal computers. Snags in the supply chain have crippled a wide swath of industries and hiked prices on some consumer goods.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://customersurvey.onl/www-lowes-ca-survey/" target="_self"&gt;&lt;SPAN&gt;https://customersurvey.onl/www-lowes-ca-survey/&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Feb 2023 08:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Missing-Processor-Expert-Component-Property/m-p/1593770#M5447</guid>
      <dc:creator>denial234</dc:creator>
      <dc:date>2023-02-06T08:18:30Z</dc:date>
    </item>
  </channel>
</rss>