<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: how to format sd card  from images which generated yocto? in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/how-to-format-sd-card-from-images-which-generated-yocto/m-p/1399245#M4948</link>
    <description>&lt;P&gt;Please refer to this thread.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Layerscape/How-to-create-a-bootable-SD-for-the-LS1043ARDB/m-p/1297151#M8270" target="_blank"&gt;https://community.nxp.com/t5/Layerscape/How-to-create-a-bootable-SD-for-the-LS1043ARDB/m-p/1297151#M8270&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 14 Jan 2022 04:51:38 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-01-14T04:51:38Z</dc:date>
    <item>
      <title>how to format sd card  from images which generated yocto?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/how-to-format-sd-card-from-images-which-generated-yocto/m-p/1397336#M4943</link>
      <description>&lt;P&gt;Images can be found&amp;nbsp; under /tmp/deploys/images&lt;/P&gt;&lt;P&gt;how to format sd card from the images ?&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jan 2022 10:35:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/how-to-format-sd-card-from-images-which-generated-yocto/m-p/1397336#M4943</guid>
      <dc:creator>fenghua_jiang</dc:creator>
      <dc:date>2022-01-11T10:35:30Z</dc:date>
    </item>
    <item>
      <title>Re: how to format sd card  from images which generated yocto?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/how-to-format-sd-card-from-images-which-generated-yocto/m-p/1399245#M4948</link>
      <description>&lt;P&gt;Please refer to this thread.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Layerscape/How-to-create-a-bootable-SD-for-the-LS1043ARDB/m-p/1297151#M8270" target="_blank"&gt;https://community.nxp.com/t5/Layerscape/How-to-create-a-bootable-SD-for-the-LS1043ARDB/m-p/1297151#M8270&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jan 2022 04:51:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/how-to-format-sd-card-from-images-which-generated-yocto/m-p/1399245#M4948</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-01-14T04:51:38Z</dc:date>
    </item>
    <item>
      <title>Re: how to format sd card  from images which generated yocto?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/how-to-format-sd-card-from-images-which-generated-yocto/m-p/1409944#M4986</link>
      <description>&lt;P&gt;follow &lt;A href="https://community.nxp.com/t5/Layerscape/How-to-create-a-bootable-SD-for-the-LS1043ARDB/m-p/1297151#M8270" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/Layerscape/How-to-create-a-bootable-SD-for-the-LS1043ARDB/m-p/1297151#M...&lt;/A&gt;&lt;/P&gt;&lt;P&gt;# mkfs.vfat /dev/sdb1&lt;BR /&gt;# mkfs.ext2 /dev/sdb2&lt;/P&gt;&lt;P&gt;sdb 8:16 1 14.9G 0 disk&lt;BR /&gt;├─sdb1 8:17 1 1G 0 part&lt;BR /&gt;└─sdb2 8:18 1 13.8G 0 part&lt;/P&gt;&lt;P&gt;after&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;sudo dd if=bl2_sd.pbl of=/dev/sdb bs=512 seek=8&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;sudo dd if=bl2_sd.pbl of=/dev/sdb bs=512 seek=8&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;sudo dd if=fsl_fman_ucode_ls1043_r1.1_106_4_18.bin of=/dev/sdb bs=512 seek=18432&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;the options of sdb was destroyed.&lt;/P&gt;&lt;P&gt;Command (m for help): p&lt;BR /&gt;Disk /dev/sdb: 14.9 GiB, 15931539456 bytes, 31116288 sectors&lt;BR /&gt;Units: sectors of 1 * 512 = 512 bytes&lt;BR /&gt;Sector size (logical/physical): 512 bytes / 512 bytes&lt;BR /&gt;I/O size (minimum/optimal): 512 bytes / 512 bytes&lt;BR /&gt;Disklabel type: dos&lt;BR /&gt;Disk identifier: 0x6b81d535&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Feb 2022 03:18:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/how-to-format-sd-card-from-images-which-generated-yocto/m-p/1409944#M4986</guid>
      <dc:creator>fenghua_jiang</dc:creator>
      <dc:date>2022-02-08T03:18:04Z</dc:date>
    </item>
    <item>
      <title>Re: how to format sd card  from images which generated yocto?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/how-to-format-sd-card-from-images-which-generated-yocto/m-p/1412114#M4994</link>
      <description>&lt;P&gt;1. Please create two partitions with Linux command "fdisk", one 1G FAT16 and 2G one ext2/ext3 or with remainder of the available disk size.&lt;BR /&gt;# mkfs.vfat /dev/sdb1&lt;BR /&gt;# mkfs.ext2 /dev/sdb2&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;2. Please deployed RCW + PBI + BL2(bl2_&amp;lt;boot_mode&amp;gt;.pbl)image to SD card as the following.&lt;BR /&gt;dd if=bl2_sd.pbl of=/dev/sdb bs=512 seek=8&lt;/P&gt;&lt;P&gt;note:/dev/sdb is SD device name.&lt;/P&gt;&lt;P&gt;Please deploy TF-A FIP image at 0x00800 in SD card.&lt;/P&gt;&lt;P&gt;dd if=fip_uboot.bin of=/dev/sdb bs=512 seek=0x800&lt;/P&gt;&lt;P&gt;Please deploy FMAN ucode at 0x04800 in SD card.&lt;/P&gt;&lt;P&gt;dd if=fsl_fman_ucode_ls1043_r1.1_106_4_18.bin of=/dev/sdb bs=512 seek=0x4800&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="6"&gt;&lt;STRONG&gt;&lt;EM&gt;you can't find /dev/sdb2&lt;/EM&gt;&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Feb 2022 01:53:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/how-to-format-sd-card-from-images-which-generated-yocto/m-p/1412114#M4994</guid>
      <dc:creator>fenghua_jiang</dc:creator>
      <dc:date>2022-02-11T01:53:30Z</dc:date>
    </item>
    <item>
      <title>Re: how to format sd card  from images which generated yocto?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/how-to-format-sd-card-from-images-which-generated-yocto/m-p/1412246#M4995</link>
      <description>&lt;P&gt;Set the environment in uboot for SD boot.:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;setenv bootcmd 'setenv bootargs root=/dev/mmcblk0p2 rw rootdelay=5 console=ttyS0,115200;mmcinfo;ext2load mmc 0:2 0xa0000000 /boot/Image;ext2load mmc 0:2 0xb0000000 /boot/fsl-ls1043a-rdb-sdk.dtb;booti 0xa0000000- 0xb0000000'&lt;/P&gt;&lt;P&gt;saveenv&lt;/P&gt;&lt;P&gt;boot&lt;/P&gt;&lt;P&gt;Moving Image from 0xa0000000 to 0xa0080000, end=a15d6000&lt;BR /&gt;## Loading ramdisk from FIT Image at b0000000 ...&lt;BR /&gt;Bad FIT ramdisk image format! (err=-42)&lt;BR /&gt;Ramdisk image is corrupt or invalid&lt;/P&gt;</description>
      <pubDate>Fri, 11 Feb 2022 06:50:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/how-to-format-sd-card-from-images-which-generated-yocto/m-p/1412246#M4995</guid>
      <dc:creator>fenghua_jiang</dc:creator>
      <dc:date>2022-02-11T06:50:25Z</dc:date>
    </item>
    <item>
      <title>Re: how to format sd card  from images which generated yocto?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/how-to-format-sd-card-from-images-which-generated-yocto/m-p/1412333#M4996</link>
      <description>&lt;P&gt;Would you please post your whole procedure here?&lt;/P&gt;</description>
      <pubDate>Fri, 11 Feb 2022 09:06:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/how-to-format-sd-card-from-images-which-generated-yocto/m-p/1412333#M4996</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-02-11T09:06:10Z</dc:date>
    </item>
  </channel>
</rss>