<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 Generate Code from specified Processor Expert</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Generate-Code-from-specified-Processor-Expert/m-p/1316038#M4900</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In my project I have two processor experts. How would I specify which processor expert to generate code from?&lt;/P&gt;&lt;P&gt;If I have two PE files, PExpertV0.pe, PExpertV1.pe. Although I click on Generate code from PExpertV1.pe, the code for PExpertV0.pe gets generated.&lt;/P&gt;&lt;P&gt;Also, command line interface for generation doesn't work.&lt;/P&gt;&lt;P&gt;I run the following command there are no errors but no files are generated:&lt;/P&gt;&lt;P&gt;eclipsec.exe -noSplash -data C:\Repo\XYZ -application com.freescale.processorexpert.core.PExApplication -generateAll&lt;/P&gt;&lt;P&gt;Overall I would like to&lt;/P&gt;&lt;P&gt;If HW_VARIANT == XXXX&lt;/P&gt;&lt;P&gt;Generate ProcessorExpertV0.pe&lt;/P&gt;&lt;P&gt;else if HW_VARIANT = YYYY&lt;/P&gt;&lt;P&gt;Generate ProecssorExpertV1.pe&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 30 Jul 2021 15:13:24 GMT</pubDate>
    <dc:creator>ShriraamSundaram</dc:creator>
    <dc:date>2021-07-30T15:13:24Z</dc:date>
    <item>
      <title>Generate Code from specified Processor Expert</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Generate-Code-from-specified-Processor-Expert/m-p/1316038#M4900</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In my project I have two processor experts. How would I specify which processor expert to generate code from?&lt;/P&gt;&lt;P&gt;If I have two PE files, PExpertV0.pe, PExpertV1.pe. Although I click on Generate code from PExpertV1.pe, the code for PExpertV0.pe gets generated.&lt;/P&gt;&lt;P&gt;Also, command line interface for generation doesn't work.&lt;/P&gt;&lt;P&gt;I run the following command there are no errors but no files are generated:&lt;/P&gt;&lt;P&gt;eclipsec.exe -noSplash -data C:\Repo\XYZ -application com.freescale.processorexpert.core.PExApplication -generateAll&lt;/P&gt;&lt;P&gt;Overall I would like to&lt;/P&gt;&lt;P&gt;If HW_VARIANT == XXXX&lt;/P&gt;&lt;P&gt;Generate ProcessorExpertV0.pe&lt;/P&gt;&lt;P&gt;else if HW_VARIANT = YYYY&lt;/P&gt;&lt;P&gt;Generate ProecssorExpertV1.pe&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jul 2021 15:13:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Generate-Code-from-specified-Processor-Expert/m-p/1316038#M4900</guid>
      <dc:creator>ShriraamSundaram</dc:creator>
      <dc:date>2021-07-30T15:13:24Z</dc:date>
    </item>
  </channel>
</rss>