<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Processor Expert Internal Oscillator Frequency Trim Value Initialization in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-Internal-Oscillator-Frequency-Trim-Value/m-p/1365466#M4895</link>
    <description>&lt;P&gt;Thanks for the suggestion.&lt;/P&gt;</description>
    <pubDate>Wed, 03 Nov 2021 05:32:02 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2021-11-03T05:32:02Z</dc:date>
    <item>
      <title>Processor Expert Internal Oscillator Frequency Trim Value Initialization</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-Internal-Oscillator-Frequency-Trim-Value/m-p/1227821#M4852</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;According to the problem in post: &lt;A href="https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SCI-baudrate-veriation-when-flashing/m-p/1227780/highlight/false#M23267" target="_blank"&gt;https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SCI-baudrate-veriation-when-flashing/m-p/1227780/highlight/false#M23267&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I realized that the Processor Expert does not initialize the trim value of the internal oscillator, only gives the option to assign a fixed memory position to allocate the value. When debugging, it seems that the trim values are automatically inserted, but not when flashing, so it has to be done by "hand".&lt;/P&gt;&lt;P&gt;As in PE the frequency value is selectable, I propose to assign the correct values in the code generated by the PE.&lt;/P&gt;&lt;P&gt;I have seen this issue with the MC9S08QG8 micro controller and Codewarrior V11, so the registers affected would be ICSTRM and ICSSC to be included at file CPU.c.&lt;/P&gt;&lt;P&gt;Thank you and regards.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Feb 2021 08:53:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-Internal-Oscillator-Frequency-Trim-Value/m-p/1227821#M4852</guid>
      <dc:creator>egoitztoledo</dc:creator>
      <dc:date>2021-02-08T08:53:31Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert Internal Oscillator Frequency Trim Value Initialization</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-Internal-Oscillator-Frequency-Trim-Value/m-p/1365466#M4895</link>
      <description>&lt;P&gt;Thanks for the suggestion.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Nov 2021 05:32:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-Internal-Oscillator-Frequency-Trim-Value/m-p/1365466#M4895</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-11-03T05:32:02Z</dc:date>
    </item>
  </channel>
</rss>