<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Open-drain for alternate function LPC17XX in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Open-drain-for-alternate-function-LPC17XX/m-p/1362639#M4886</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The GPIO&amp;nbsp; pins are only configurable in pull-up/down resistors, open drain mode, and repeater mode. The I2C is a dedicated open-drain pins without pull-up/down.&lt;/P&gt;
&lt;P&gt;The open drain SPI option is not implemented in this design LPC17xx.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;In conclusion the GPIO can only be set in open-drain mode.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 27 Oct 2021 18:46:23 GMT</pubDate>
    <dc:creator>nxf77486</dc:creator>
    <dc:date>2021-10-27T18:46:23Z</dc:date>
    <item>
      <title>Open-drain for alternate function LPC17XX</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Open-drain-for-alternate-function-LPC17XX/m-p/1361710#M4880</link>
      <description>&lt;P&gt;Hi everyone&lt;/P&gt;&lt;P&gt;I am trying to set pins SCK0 and MOSI0(BRIDGE 1) in open-drain mode for microntroller 1752 but setting the register&amp;nbsp;LPC_PINCON-&amp;gt;PINMODE_OD1 to open drain does not seem to work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Clock Pin: P1[20]/MCI0/PWM1[2]/&lt;STRONG&gt;SCK0&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Data Pin:&amp;nbsp;P1[24]/MCI2/PWM1[5]/&lt;STRONG&gt;MOSI0&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;LPC_PINCON-&amp;gt;PINMODE_OD1 |= 1&amp;lt;&amp;lt;20; //Bit P1.20 is open drain&lt;BR /&gt;LPC_PINCON-&amp;gt;PINMODE_OD1 |= 1&amp;lt;&amp;lt;24; //Bit P1.24 is open drain&lt;/P&gt;&lt;P&gt;If I configure the pin as GPIO the pin is set in open-drain.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If there any way to set a non-GPIO pin in open-drain mode?&lt;/P&gt;&lt;P&gt;Thank you.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Oct 2021 13:31:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Open-drain-for-alternate-function-LPC17XX/m-p/1361710#M4880</guid>
      <dc:creator>xvidaurrazaga</dc:creator>
      <dc:date>2021-10-26T13:31:28Z</dc:date>
    </item>
    <item>
      <title>Re: Open-drain for alternate function LPC17XX</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Open-drain-for-alternate-function-LPC17XX/m-p/1362639#M4886</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The GPIO&amp;nbsp; pins are only configurable in pull-up/down resistors, open drain mode, and repeater mode. The I2C is a dedicated open-drain pins without pull-up/down.&lt;/P&gt;
&lt;P&gt;The open drain SPI option is not implemented in this design LPC17xx.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;In conclusion the GPIO can only be set in open-drain mode.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 18:46:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Open-drain-for-alternate-function-LPC17XX/m-p/1362639#M4886</guid>
      <dc:creator>nxf77486</dc:creator>
      <dc:date>2021-10-27T18:46:23Z</dc:date>
    </item>
    <item>
      <title>Re: Open-drain for alternate function LPC17XX</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Open-drain-for-alternate-function-LPC17XX/m-p/1362987#M4888</link>
      <description>&lt;P&gt;thank you so much for your reply&lt;/P&gt;</description>
      <pubDate>Thu, 28 Oct 2021 06:10:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Open-drain-for-alternate-function-LPC17XX/m-p/1362987#M4888</guid>
      <dc:creator>xvidaurrazaga</dc:creator>
      <dc:date>2021-10-28T06:10:22Z</dc:date>
    </item>
  </channel>
</rss>