<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Memory copy using load multiple instruction (LMW) in T2080 in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Memory-copy-using-load-multiple-instruction-LMW-in-T2080/m-p/1338641#M4817</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to improve the memory copy performance from to/from the device attached to the PCIe interface , processor is T2080 , core is e6500.&amp;nbsp;&lt;BR /&gt;I can achieve the desired performance when i configure the PCIe BAR address space as cacheable but due to some restriction i should not make it&lt;BR /&gt;cacheable and need to transmit / receive data without caching.&lt;/P&gt;&lt;P&gt;I am thinking to make the c routine which uses the load multiple instruction (LMW) for memory copy.&lt;BR /&gt;Can i get some reference how to use this instruction in C routine for this task ?&lt;BR /&gt;OR if any other ideas to make it easier ?&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Vijay&lt;/P&gt;</description>
    <pubDate>Sun, 12 Sep 2021 02:56:25 GMT</pubDate>
    <dc:creator>veejppee</dc:creator>
    <dc:date>2021-09-12T02:56:25Z</dc:date>
    <item>
      <title>Memory copy using load multiple instruction (LMW) in T2080</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Memory-copy-using-load-multiple-instruction-LMW-in-T2080/m-p/1338641#M4817</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to improve the memory copy performance from to/from the device attached to the PCIe interface , processor is T2080 , core is e6500.&amp;nbsp;&lt;BR /&gt;I can achieve the desired performance when i configure the PCIe BAR address space as cacheable but due to some restriction i should not make it&lt;BR /&gt;cacheable and need to transmit / receive data without caching.&lt;/P&gt;&lt;P&gt;I am thinking to make the c routine which uses the load multiple instruction (LMW) for memory copy.&lt;BR /&gt;Can i get some reference how to use this instruction in C routine for this task ?&lt;BR /&gt;OR if any other ideas to make it easier ?&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Vijay&lt;/P&gt;</description>
      <pubDate>Sun, 12 Sep 2021 02:56:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Memory-copy-using-load-multiple-instruction-LMW-in-T2080/m-p/1338641#M4817</guid>
      <dc:creator>veejppee</dc:creator>
      <dc:date>2021-09-12T02:56:25Z</dc:date>
    </item>
    <item>
      <title>Re: Memory copy using load multiple instruction (LMW) in T2080</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Memory-copy-using-load-multiple-instruction-LMW-in-T2080/m-p/1352338#M4855</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Why DMA is not used for memory copy?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Oct 2021 05:33:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Memory-copy-using-load-multiple-instruction-LMW-in-T2080/m-p/1352338#M4855</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-10-08T05:33:08Z</dc:date>
    </item>
  </channel>
</rss>