<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic P.E K70 TWR UART3 Can't get input from terminal. in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/P-E-K70-TWR-UART3-Can-t-get-input-from-terminal/m-p/182905#M480</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have wired UART3 out of a TWO-PROTO board. I created a PE Embeeded device for UART3. My code uses UART3 because I can see AS1_Blocks being sent from the code. But, even though I have a clean signal going into pin A41 of the riser cards I can not get any received block events from UART3.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I added 0 ohm resistors for R134, R135 and I am not using a LCDD3, D4 for anything.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please advise. It is somewhat urgent.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Jul 2012 03:17:23 GMT</pubDate>
    <dc:creator>crezyoz</dc:creator>
    <dc:date>2012-07-25T03:17:23Z</dc:date>
    <item>
      <title>P.E K70 TWR UART3 Can't get input from terminal.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/P-E-K70-TWR-UART3-Can-t-get-input-from-terminal/m-p/182905#M480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have wired UART3 out of a TWO-PROTO board. I created a PE Embeeded device for UART3. My code uses UART3 because I can see AS1_Blocks being sent from the code. But, even though I have a clean signal going into pin A41 of the riser cards I can not get any received block events from UART3.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I added 0 ohm resistors for R134, R135 and I am not using a LCDD3, D4 for anything.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please advise. It is somewhat urgent.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jul 2012 03:17:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/P-E-K70-TWR-UART3-Can-t-get-input-from-terminal/m-p/182905#M480</guid>
      <dc:creator>crezyoz</dc:creator>
      <dc:date>2012-07-25T03:17:23Z</dc:date>
    </item>
    <item>
      <title>Re: P.E K70 TWR UART3 Can't get input from terminal.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/P-E-K70-TWR-UART3-Can-t-get-input-from-terminal/m-p/182906#M481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did a test by calling&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;AS1_ReceiveBlock(AS1_DeviceData , rcvBlk,4))&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and in fact, after 4 transmits, it did register that data had been received. And the receiveBlock even was triggered. Seems the event only gets triggered if I call AS1_ReceiveBlock. Hmmmm..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jul 2012 04:20:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/P-E-K70-TWR-UART3-Can-t-get-input-from-terminal/m-p/182906#M481</guid>
      <dc:creator>crezyoz</dc:creator>
      <dc:date>2012-07-25T04:20:57Z</dc:date>
    </item>
    <item>
      <title>Re: P.E K70 TWR UART3 Can't get input from terminal.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/P-E-K70-TWR-UART3-Can-t-get-input-from-terminal/m-p/182907#M482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I suppose you are using Seial_LDD component. Please check the examples of code on the "Typical usage" page in the help for the component. It can be opened using the pop-up menu command "Help on Component" and selecting "Typical usage" in the links list on the left.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Petr Hradsky&lt;BR /&gt;Processor Expert Support Team&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jul 2012 19:53:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/P-E-K70-TWR-UART3-Can-t-get-input-from-terminal/m-p/182907#M482</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2012-07-27T19:53:41Z</dc:date>
    </item>
  </channel>
</rss>