<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 Re: IMX8qm-mek can0 using for J1939</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/IMX8qm-mek-can0-using-for-J1939/m-p/1294389#M4747</link>
    <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;I will check and update for the same.&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Subbu&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 18 Jun 2021 03:38:41 GMT</pubDate>
    <dc:creator>rahulM</dc:creator>
    <dc:date>2021-06-18T03:38:41Z</dc:date>
    <item>
      <title>IMX8qm-mek can0 using for J1939</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/IMX8qm-mek-can0-using-for-J1939/m-p/1294089#M4744</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;I am using CAN-0 for J1939 protocol,&lt;/P&gt;&lt;P&gt;I am not able to read CAN data and pgn from the busmaster.&lt;/P&gt;&lt;P&gt;I am using i.MX Linux Yocto Project BSP 5.4.47_2.2.0 Release.&lt;/P&gt;&lt;P&gt;I added can-utils in conf file and enabled CONFIG_CAN_J1939.&lt;/P&gt;&lt;P&gt;I referred&amp;nbsp;&lt;A href="https://github.com/linux-can/can-utils/blob/master/testj1939.c" target="_blank"&gt;https://github.com/linux-can/can-utils/blob/master/testj1939.c&lt;/A&gt;&amp;nbsp;still not able to r/w.&lt;/P&gt;&lt;P&gt;Please share any sample J1939 linux based application code to read/write from the busmaster simulator.&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Subbu&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jun 2021 12:18:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/IMX8qm-mek-can0-using-for-J1939/m-p/1294089#M4744</guid>
      <dc:creator>rahulM</dc:creator>
      <dc:date>2021-06-17T12:18:41Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8qm-mek can0 using for J1939</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/IMX8qm-mek-can0-using-for-J1939/m-p/1294322#M4746</link>
      <description>&lt;P&gt;Hi Subbu&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If default images for Linux were used, please check if M4 was started. In affirmative case, CAN Resources are assigned to M4 and this can determine Linux CAN driver not to probe.&lt;/P&gt;
&lt;P&gt;If this is the case, there are 2 possibilities:&lt;/P&gt;
&lt;P&gt;1. M4 is not needed ==&amp;gt; use a flash.bin without M4 firmware (imx-boot-imx8qmmek-sd.bin-flash_linux)&lt;/P&gt;
&lt;P&gt;2. Otherwise, M4 Resources has to be unassigned from M4 partition (board.c of SCFW).&lt;/P&gt;
&lt;P&gt;Example can be found on below link&amp;nbsp; sect. "Modifying default configuration" :&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Resource-management-service/ta-p/1123227" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Resource-management-service/ta-p/1123227&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;From Linux Kernel perspective, the nodes are enabled in dts:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm-mek.dts?h=imx_5.4.47_2.2.0" target="_blank" rel="noopener"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm-mek.dts?h=imx_5.4.47_2.2.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;Please share any sample J1939 linux based application code to read/write from the busmaster simulator.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;sorry such example is not available.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 18 Jun 2021 00:36:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/IMX8qm-mek-can0-using-for-J1939/m-p/1294322#M4746</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-06-18T00:36:15Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8qm-mek can0 using for J1939</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/IMX8qm-mek-can0-using-for-J1939/m-p/1294389#M4747</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;I will check and update for the same.&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Subbu&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Jun 2021 03:38:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/IMX8qm-mek-can0-using-for-J1939/m-p/1294389#M4747</guid>
      <dc:creator>rahulM</dc:creator>
      <dc:date>2021-06-18T03:38:41Z</dc:date>
    </item>
  </channel>
</rss>