<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8M Nano :- How to boot from USB? in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/IMX8M-Nano-How-to-boot-from-USB/m-p/1226382#M4608</link>
    <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/171173"&gt;@AldoG&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank You For Your Reply.&lt;/P&gt;&lt;P&gt;In terms of hardware, we have just copy eMMC,DDR and MPU Connections in the schematic from imx8m nano EVK (SPF-45699_A2.pdf).&lt;/P&gt;&lt;P&gt;We have used "&lt;STRONG&gt;MIMX8MN1CVTIZAA&lt;/STRONG&gt;" MPU ,while EVK has used&amp;nbsp; "&lt;STRONG&gt;MIMX8MN6DVTJZAA&lt;/STRONG&gt;"&lt;/P&gt;&lt;P&gt;We have used "&lt;STRONG&gt;BD71847AMWV&lt;/STRONG&gt;-&lt;STRONG&gt;E2&lt;/STRONG&gt;" PMIC , While EVK has used "&lt;STRONG&gt;BD71850MWV&lt;/STRONG&gt;"&lt;/P&gt;&lt;P&gt;Does DDR4 Calibration needed for flashing images to emmc via USB?&lt;/P&gt;&lt;P&gt;Does DDR4 Calibration needed in mpu booting process?&lt;/P&gt;&lt;P&gt;I have question specific to eMMC.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Do we need pull up on eMMC(Part:- EMMC08G-T227) data and Cmd line?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Please Suggest me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 04 Feb 2021 11:41:39 GMT</pubDate>
    <dc:creator>milav_soni</dc:creator>
    <dc:date>2021-02-04T11:41:39Z</dc:date>
    <item>
      <title>IMX8M Nano :- How to boot from USB?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/IMX8M-Nano-How-to-boot-from-USB/m-p/1225441#M4604</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We have build a custom Board which have "&lt;STRONG&gt;MIMX8MN1CVTIZAA&lt;/STRONG&gt;" MPU.&lt;/P&gt;&lt;P&gt;I want to boot the board using USB mode, But i don't get any output/log in UART2 debug port.&lt;/P&gt;&lt;P&gt;I have used "0001" logic level in Boot Mode. (Boot Mode 3 to Boot Mode 0 respectively)&lt;/P&gt;&lt;P&gt;My USB OTG is connected directly to USB1_DN(A22)/USB1_DP(B22) signals and another three signals as per H/W guide.&lt;/P&gt;&lt;P&gt;Should i boot from usb pins? what is the correct process for it?&lt;/P&gt;&lt;P&gt;I am using following images to write emmc from usb.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp; &amp;nbsp; L5.4.47-2.2.0_images_MX8MNEVK&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I have tried following command via UUU, But I got error.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;sudo ./uuu uuu.auto-imx8mnevk 
[sudo] password for dell: 
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.72-0-g8e9e189

Success 0    Failure 1                                                                                                                                                 
                                                                                                                                                                        
                                                                                                                                                                        
3:10     1/ 1 [HID(W):LIBUSB_ERROR_TIMEOUT           ] SDPS: boot -f imx-boot-imx8mnevk-sd.bin-flash_evk &lt;/LI-CODE&gt;&lt;P&gt;can You please help me out on this error?&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;</description>
      <pubDate>Wed, 03 Feb 2021 10:06:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/IMX8M-Nano-How-to-boot-from-USB/m-p/1225441#M4604</guid>
      <dc:creator>milav_soni</dc:creator>
      <dc:date>2021-02-03T10:06:16Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M Nano :- How to boot from USB?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/IMX8M-Nano-How-to-boot-from-USB/m-p/1225829#M4606</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;If the board is being detected by your host PC then the USB connection is correct. You may use the following command:&lt;BR /&gt;&lt;BR /&gt;Windows host pc:&lt;BR /&gt;uuu -lsusb&lt;BR /&gt;&lt;BR /&gt;Linux host pc:&lt;BR /&gt;lsusb&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;As for the error you're seeing in the tool, this will be caused because of the uboot version you are trying to use is not compatible with your custom board.&lt;BR /&gt;&lt;BR /&gt;It is recommended to run DDR calibration first&amp;nbsp; using the DDR tool and then build your own uboot with the correct values for your design.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Feb 2021 20:39:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/IMX8M-Nano-How-to-boot-from-USB/m-p/1225829#M4606</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-02-03T20:39:45Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M Nano :- How to boot from USB?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/IMX8M-Nano-How-to-boot-from-USB/m-p/1226382#M4608</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/171173"&gt;@AldoG&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank You For Your Reply.&lt;/P&gt;&lt;P&gt;In terms of hardware, we have just copy eMMC,DDR and MPU Connections in the schematic from imx8m nano EVK (SPF-45699_A2.pdf).&lt;/P&gt;&lt;P&gt;We have used "&lt;STRONG&gt;MIMX8MN1CVTIZAA&lt;/STRONG&gt;" MPU ,while EVK has used&amp;nbsp; "&lt;STRONG&gt;MIMX8MN6DVTJZAA&lt;/STRONG&gt;"&lt;/P&gt;&lt;P&gt;We have used "&lt;STRONG&gt;BD71847AMWV&lt;/STRONG&gt;-&lt;STRONG&gt;E2&lt;/STRONG&gt;" PMIC , While EVK has used "&lt;STRONG&gt;BD71850MWV&lt;/STRONG&gt;"&lt;/P&gt;&lt;P&gt;Does DDR4 Calibration needed for flashing images to emmc via USB?&lt;/P&gt;&lt;P&gt;Does DDR4 Calibration needed in mpu booting process?&lt;/P&gt;&lt;P&gt;I have question specific to eMMC.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Do we need pull up on eMMC(Part:- EMMC08G-T227) data and Cmd line?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Please Suggest me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 11:41:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/IMX8M-Nano-How-to-boot-from-USB/m-p/1226382#M4608</guid>
      <dc:creator>milav_soni</dc:creator>
      <dc:date>2021-02-04T11:41:39Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M Nano :- How to boot from USB?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/IMX8M-Nano-How-to-boot-from-USB/m-p/1227150#M4612</link>
      <description>&lt;P&gt;Thank You For your reply.&lt;/P&gt;&lt;P&gt;I am able to write image in to emmc through USB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Feb 2021 13:12:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/IMX8M-Nano-How-to-boot-from-USB/m-p/1227150#M4612</guid>
      <dc:creator>milav_soni</dc:creator>
      <dc:date>2021-02-05T13:12:13Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M Nano :- How to boot from USB?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/IMX8M-Nano-How-to-boot-from-USB/m-p/1552941#M5321</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/65023"&gt;@milav_soni&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I am meeting this issue as your mentioned.&lt;/P&gt;&lt;P&gt;Could you help me write the image file to emmc via USB boot?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Mon, 14 Nov 2022 03:08:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/IMX8M-Nano-How-to-boot-from-USB/m-p/1552941#M5321</guid>
      <dc:creator>DinhNguyen</dc:creator>
      <dc:date>2022-11-14T03:08:55Z</dc:date>
    </item>
  </channel>
</rss>