<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックDevice firmware for 16 channel class 2 audio</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Device-firmware-for-16-channel-class-2-audio/m-p/1220045#M4592</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;We are investigating if we can use a i.MXRT MCU for our product. This product will include 16 channel audio output. So we need USB firmware that supports class 2 audio output.&lt;/P&gt;&lt;P&gt;We have seen the 'Composite CDC (serial COM) + 2-channel audio input / output' example. This seems to be an interresting starting point. But is this easily adaptable to 16 channels?&lt;/P&gt;</description>
    <pubDate>Sun, 24 Jan 2021 20:53:27 GMT</pubDate>
    <dc:creator>simmania</dc:creator>
    <dc:date>2021-01-24T20:53:27Z</dc:date>
    <item>
      <title>Device firmware for 16 channel class 2 audio</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Device-firmware-for-16-channel-class-2-audio/m-p/1220045#M4592</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;We are investigating if we can use a i.MXRT MCU for our product. This product will include 16 channel audio output. So we need USB firmware that supports class 2 audio output.&lt;/P&gt;&lt;P&gt;We have seen the 'Composite CDC (serial COM) + 2-channel audio input / output' example. This seems to be an interresting starting point. But is this easily adaptable to 16 channels?&lt;/P&gt;</description>
      <pubDate>Sun, 24 Jan 2021 20:53:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Device-firmware-for-16-channel-class-2-audio/m-p/1220045#M4592</guid>
      <dc:creator>simmania</dc:creator>
      <dc:date>2021-01-24T20:53:27Z</dc:date>
    </item>
    <item>
      <title>Re: Device firmware for 16 channel class 2 audio</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Device-firmware-for-16-channel-class-2-audio/m-p/1220126#M4593</link>
      <description>&lt;P&gt;Hi simmania,&lt;/P&gt;
&lt;P&gt;No, there isn't such examples which use more than two channel.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 03:28:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Device-firmware-for-16-channel-class-2-audio/m-p/1220126#M4593</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-01-25T03:28:33Z</dc:date>
    </item>
    <item>
      <title>Re: Device firmware for 16 channel class 2 audio</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Device-firmware-for-16-channel-class-2-audio/m-p/1220352#M4594</link>
      <description>&lt;P&gt;Will it be easy to adapt the 2 channel example to 16 channels? Like changing a few constants from 2 to 16? And off course taking care of the audio samples.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 08:27:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Device-firmware-for-16-channel-class-2-audio/m-p/1220352#M4594</guid>
      <dc:creator>simmania</dc:creator>
      <dc:date>2021-01-25T08:27:22Z</dc:date>
    </item>
  </channel>
</rss>