<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Softwareのトピックsame PIT for ADC trigger A and ADC trigger B</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/same-PIT-for-ADC-trigger-A-and-ADC-trigger-B/m-p/180715#M458</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I don't get why it's not possible. Processor expert complains that "Pins with shared control must be set identically", which I don't understand very well... Could somoene explain this message more clearly? If it's a hardware limitation, is there a workaround in order to achieve what I want to do (I want one PIT to trigger both A and B sources on both ADCs).&lt;/P&gt;&lt;P&gt;My platform is the twr-k60n512, and I use IAR + MQX + Processor expert.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you !&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;--&lt;/P&gt;&lt;P&gt;Emilien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jul 2012 21:42:57 GMT</pubDate>
    <dc:creator>emilien</dc:creator>
    <dc:date>2012-07-18T21:42:57Z</dc:date>
    <item>
      <title>same PIT for ADC trigger A and ADC trigger B</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/same-PIT-for-ADC-trigger-A-and-ADC-trigger-B/m-p/180715#M458</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I don't get why it's not possible. Processor expert complains that "Pins with shared control must be set identically", which I don't understand very well... Could somoene explain this message more clearly? If it's a hardware limitation, is there a workaround in order to achieve what I want to do (I want one PIT to trigger both A and B sources on both ADCs).&lt;/P&gt;&lt;P&gt;My platform is the twr-k60n512, and I use IAR + MQX + Processor expert.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you !&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;--&lt;/P&gt;&lt;P&gt;Emilien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2012 21:42:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/same-PIT-for-ADC-trigger-A-and-ADC-trigger-B/m-p/180715#M458</guid>
      <dc:creator>emilien</dc:creator>
      <dc:date>2012-07-18T21:42:57Z</dc:date>
    </item>
    <item>
      <title>Re: same PIT for ADC trigger A and ADC trigger B</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/same-PIT-for-ADC-trigger-A-and-ADC-trigger-B/m-p/180716#M459</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"Pins with shared control must be set identically" means some conflict in muxing/routing. The message will be improved in CW V10.3 as you can see in the attachment.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Based on the improved message and documentaiton in RM (screen-shot attached too) seems only one pre-triger is possible to select in case of not PDB trigger is used.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Vojtech Filip&lt;BR /&gt;Processor Expert Support Team&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2012 22:08:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/same-PIT-for-ADC-trigger-A-and-ADC-trigger-B/m-p/180716#M459</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2012-07-18T22:08:11Z</dc:date>
    </item>
    <item>
      <title>Re: same PIT for ADC trigger A and ADC trigger B</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/same-PIT-for-ADC-trigger-A-and-ADC-trigger-B/m-p/180717#M460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok thanks ! Actually I did try with the Programmable Device Block, but I could not have it trigger my ADCs... The Channel Status Register of the PDB shows Errors on my PDB channels (maybe because the ADC stops for debug and the PDB continues, but yet my ADC should have been triggered once, and it's not).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you see something wrong in the attached screenshot ?&lt;/P&gt;&lt;P&gt;If not, do you see another mean with which I could trigger my ADCs in hardware periodically ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;p.s: The RM says it's possible to freeze the PDB if the microcontroller is frozen, but I don't see which bit I should set.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2012 22:34:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/same-PIT-for-ADC-trigger-A-and-ADC-trigger-B/m-p/180717#M460</guid>
      <dc:creator>emilien</dc:creator>
      <dc:date>2012-07-18T22:34:41Z</dc:date>
    </item>
    <item>
      <title>Re: same PIT for ADC trigger A and ADC trigger B</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/same-PIT-for-ADC-trigger-A-and-ADC-trigger-B/m-p/180718#M461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;could you please check the project within this thread:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A __default_attr="108258" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/108258" jivemacro="thread" title="https://community.freescale.com/thread/108258"&gt;https://community.freescale.com/thread/108258&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think there is the use case you need.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Vojtech Filip&lt;BR /&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2012 13:48:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/same-PIT-for-ADC-trigger-A-and-ADC-trigger-B/m-p/180718#M461</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2012-07-19T13:48:27Z</dc:date>
    </item>
    <item>
      <title>Re: same PIT for ADC trigger A and ADC trigger B</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/same-PIT-for-ADC-trigger-A-and-ADC-trigger-B/m-p/180719#M462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; On your init_adc.png screen you have PIT_trigger_0 as the trigger A soruce and PIT_trigger_1 as the trigger B source, does the same error occur if you set both to PIT_trigger_0 ? On mine I do have the same error, which I don't understand.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;About the PDB trigger, I could not manage to trigger my ADCs, and I already checked this project but was not able to replicate it. I noticed some other people are experiencing the same issue (&lt;A __default_attr="115730" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/115730" jivemacro="thread" title="https://community.freescale.com/thread/115730"&gt;https://community.freescale.com/thread/115730&lt;/A&gt; so maybe there is an underlying problem here ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2012 15:34:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/same-PIT-for-ADC-trigger-A-and-ADC-trigger-B/m-p/180719#M462</guid>
      <dc:creator>emilien</dc:creator>
      <dc:date>2012-07-19T15:34:52Z</dc:date>
    </item>
  </channel>
</rss>