<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 Restart status register RCM SRS1 Jtag bit</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Restart-status-register-RCM-SRS1-Jtag-bit/m-p/1195496#M4574</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;BR /&gt;I have problem with random restarts is trying to figure out the reason.&lt;BR /&gt;I'm using a K66 Kinnetis with a jlink segger base debugger using jtag chain.&lt;/P&gt;&lt;P&gt;I run in debug mode and catch restart in the reset interrupt handler.&lt;/P&gt;&lt;P&gt;The RCM SRS1 jtag bit i set and documentation say:&lt;/P&gt;&lt;P&gt;Indicates a reset has been caused by JTAG selection of certain IR codes: EZPORT, EXTEST, HIGHZ,&lt;BR /&gt;and CLAMP.&lt;/P&gt;&lt;P&gt;Is there more info to get or is that it?&lt;/P&gt;</description>
    <pubDate>Tue, 08 Dec 2020 12:44:02 GMT</pubDate>
    <dc:creator>viktorkarlsson</dc:creator>
    <dc:date>2020-12-08T12:44:02Z</dc:date>
    <item>
      <title>Restart status register RCM SRS1 Jtag bit</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Restart-status-register-RCM-SRS1-Jtag-bit/m-p/1195496#M4574</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;BR /&gt;I have problem with random restarts is trying to figure out the reason.&lt;BR /&gt;I'm using a K66 Kinnetis with a jlink segger base debugger using jtag chain.&lt;/P&gt;&lt;P&gt;I run in debug mode and catch restart in the reset interrupt handler.&lt;/P&gt;&lt;P&gt;The RCM SRS1 jtag bit i set and documentation say:&lt;/P&gt;&lt;P&gt;Indicates a reset has been caused by JTAG selection of certain IR codes: EZPORT, EXTEST, HIGHZ,&lt;BR /&gt;and CLAMP.&lt;/P&gt;&lt;P&gt;Is there more info to get or is that it?&lt;/P&gt;</description>
      <pubDate>Tue, 08 Dec 2020 12:44:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Restart-status-register-RCM-SRS1-Jtag-bit/m-p/1195496#M4574</guid>
      <dc:creator>viktorkarlsson</dc:creator>
      <dc:date>2020-12-08T12:44:02Z</dc:date>
    </item>
    <item>
      <title>Re: Restart status register RCM SRS1 Jtag bit</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Restart-status-register-RCM-SRS1-Jtag-bit/m-p/1196900#M4575</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This issue may be caused by hardware. I suggest you make sure that the external pull up/down resistors are connected to the circuit.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 09 Dec 2020 20:56:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Restart-status-register-RCM-SRS1-Jtag-bit/m-p/1196900#M4575</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2020-12-09T20:56:30Z</dc:date>
    </item>
  </channel>
</rss>