<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Flash Command complete interrupt receiving in loop. Stopped after handling Read Collision interrupt. in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Flash-Command-complete-interrupt-receiving-in-loop-Stopped-after/m-p/1153480#M4521</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;While writing/erasing flash at some random instance controller was continuously arriving in Flash Command Complete Interrupt. The behavior was very random and occurring very rarely.&lt;/P&gt;&lt;P&gt;While searching for solution I observed that same ISR was mentioned for flash command complete and read collision error interrupt in Vector table (vector.c). Both cases are seemed to be handled in ISR too. But while writing and erasing flash only command complete interrupt is enabled/disabled but not Read Collision interrupt. When I added enabling and disabling of Read Collision interrupt in parallel to Command Complete interrupt the issue was observed to be resolved. So I have following questions:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Why only ISR assignment for read collision error interrupt? It was not enabled by default.&lt;/LI&gt;&lt;LI&gt;Is there any other reason for particular behavior?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;BR /&gt;Controller: K10_100 Series controller without FlexMemory.&lt;/P&gt;&lt;P&gt;Processor Expert Version:&amp;nbsp;Driver Suite v10.4&lt;/P&gt;</description>
    <pubDate>Tue, 15 Sep 2020 12:13:07 GMT</pubDate>
    <dc:creator>tanmay</dc:creator>
    <dc:date>2020-09-15T12:13:07Z</dc:date>
    <item>
      <title>Flash Command complete interrupt receiving in loop. Stopped after handling Read Collision interrupt.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Flash-Command-complete-interrupt-receiving-in-loop-Stopped-after/m-p/1153480#M4521</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;While writing/erasing flash at some random instance controller was continuously arriving in Flash Command Complete Interrupt. The behavior was very random and occurring very rarely.&lt;/P&gt;&lt;P&gt;While searching for solution I observed that same ISR was mentioned for flash command complete and read collision error interrupt in Vector table (vector.c). Both cases are seemed to be handled in ISR too. But while writing and erasing flash only command complete interrupt is enabled/disabled but not Read Collision interrupt. When I added enabling and disabling of Read Collision interrupt in parallel to Command Complete interrupt the issue was observed to be resolved. So I have following questions:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Why only ISR assignment for read collision error interrupt? It was not enabled by default.&lt;/LI&gt;&lt;LI&gt;Is there any other reason for particular behavior?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;BR /&gt;Controller: K10_100 Series controller without FlexMemory.&lt;/P&gt;&lt;P&gt;Processor Expert Version:&amp;nbsp;Driver Suite v10.4&lt;/P&gt;</description>
      <pubDate>Tue, 15 Sep 2020 12:13:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Flash-Command-complete-interrupt-receiving-in-loop-Stopped-after/m-p/1153480#M4521</guid>
      <dc:creator>tanmay</dc:creator>
      <dc:date>2020-09-15T12:13:07Z</dc:date>
    </item>
    <item>
      <title>Flash Command complete interrupt receiving in loop. Stopped after handling Read Collision interrupt.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Flash-Command-complete-interrupt-receiving-in-loop-Stopped-after/m-p/1155661#M4526</link>
      <description>&lt;P&gt;Hello Tanmay,&lt;/P&gt;
&lt;P&gt;As you may notice, since you only have one flash controller and to ensure the information stored in the memory is reliable, is recommendable to use one flash operation at the time. If you have more than one, the information stored could not be reliable and that could be the reason is not enabled by default&lt;/P&gt;
&lt;P&gt;So be careful with the flash operations that this not use the same flash space.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2020 16:18:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Flash-Command-complete-interrupt-receiving-in-loop-Stopped-after/m-p/1155661#M4526</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-09-18T16:18:18Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Command complete interrupt receiving in loop. Stopped after handling Read Collision interr</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Flash-Command-complete-interrupt-receiving-in-loop-Stopped-after/m-p/1155797#M4527</link>
      <description>&lt;P&gt;Thank you. Flash read writes are implemented in the code generated by Processor Expert. But isn't read collision error is to avoid such case?&lt;/P&gt;</description>
      <pubDate>Sat, 19 Sep 2020 05:41:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Flash-Command-complete-interrupt-receiving-in-loop-Stopped-after/m-p/1155797#M4527</guid>
      <dc:creator>tanmay</dc:creator>
      <dc:date>2020-09-19T05:41:53Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Command complete interrupt receiving in loop. Stopped after handling Read Collision interr</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Flash-Command-complete-interrupt-receiving-in-loop-Stopped-after/m-p/1156539#M4528</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/177995"&gt;@tanmay&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;This is only to notify if there was a flash operation while you called another one if you look at the Flash_main and see the condition, it only returns to the main if this kind of error happens to not overlap flash operations.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2020 22:53:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Flash-Command-complete-interrupt-receiving-in-loop-Stopped-after/m-p/1156539#M4528</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-09-21T22:53:11Z</dc:date>
    </item>
  </channel>
</rss>