<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: S32K142 FLEXCAN low power modes</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/S32K142-FLEXCAN-low-power-modes/m-p/1092079#M4514</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Julian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.- Some APIs that help you to enter a low power mode for the module&amp;nbsp;FLEXCAN_DRV_ConfigPN and the FLEXCAN_EnterFreezeMode but if you want to put the MCU in a low power mode you will need a power manager component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.- As it mentions in the section 55.5.11.4 Pretended Networking mode, you can put the MCU in stop mode and wake up using the Flexcan interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Jun 2020 20:55:54 GMT</pubDate>
    <dc:creator>Alexis_A</dc:creator>
    <dc:date>2020-06-04T20:55:54Z</dc:date>
    <item>
      <title>S32K142 FLEXCAN low power modes</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/S32K142-FLEXCAN-low-power-modes/m-p/1092078#M4513</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/discussion/html_S32K142\index.html"&gt;S32K142&lt;/A&gt;&amp;nbsp;with S32&amp;nbsp;SDK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Using the CAN PAL component from Processor Expert, are there any APIs that allow us to put the FlexCAN hardware into a low power mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) If I am using the FLEXCAN driver component from Processor Expert instead, there is an API called &lt;SPAN style="color: #253555; background-color: #e2e8f2; font-weight: bold; font-size: 14px;"&gt;FLEXCAN_DRV_ConfigPN()&amp;nbsp;&lt;/SPAN&gt;that lets me put the hardware into Pretended Mode which is a low power mode. But if I would like to use an even lower power mode (similar to the Sleep mode of the MSCAN of the S9KEA), is this possible?&amp;nbsp;Can&amp;nbsp;I make the CAN hardware to go to sleep (not trying to match CAN IDs) and then generate an interrupt that wakes the CPU from Stop mode when there is a change at the RX pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry if I missed this information from the documentation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 May 2020 07:05:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/S32K142-FLEXCAN-low-power-modes/m-p/1092078#M4513</guid>
      <dc:creator>julian_yeoh</dc:creator>
      <dc:date>2020-05-15T07:05:23Z</dc:date>
    </item>
    <item>
      <title>Re: S32K142 FLEXCAN low power modes</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/S32K142-FLEXCAN-low-power-modes/m-p/1092079#M4514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Julian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.- Some APIs that help you to enter a low power mode for the module&amp;nbsp;FLEXCAN_DRV_ConfigPN and the FLEXCAN_EnterFreezeMode but if you want to put the MCU in a low power mode you will need a power manager component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.- As it mentions in the section 55.5.11.4 Pretended Networking mode, you can put the MCU in stop mode and wake up using the Flexcan interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2020 20:55:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/S32K142-FLEXCAN-low-power-modes/m-p/1092079#M4514</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-06-04T20:55:54Z</dc:date>
    </item>
  </channel>
</rss>