<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: Prototype using MC9S12XEP100 based on VB9S12XEP100</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Prototype-using-MC9S12XEP100-based-on-VB9S12XEP100/m-p/1039935#M4480</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&lt;BR /&gt;You can refer to this application note:&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN3262.pdf"&gt;AN3262 Designing Hardware for the MC9S12X D-Family&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107388iD54AB24C9FD35FDA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2.&lt;BR /&gt;No, these are outputs not inputs of the internal voltage regulator.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107543i60EAB112E888C2F1/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107427i4460C5310423C7D3/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.&lt;/P&gt;&lt;P&gt;It is an addition option, if you need to use an external oscillator for some reasons.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 May 2020 11:03:01 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2020-05-19T11:03:01Z</dc:date>
    <item>
      <title>Prototype using MC9S12XEP100 based on VB9S12XEP100</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Prototype-using-MC9S12XEP100-based-on-VB9S12XEP100/m-p/1039934#M4479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm designing a prototype that uses the MC9S12XEP100 microcontroller and&amp;nbsp; I'm taking as an example the EVB9S12XEP100 evaluation board. The following questions have arisen.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;1) Regarding decoupling capacitors, I used the information present in the datasheet, mainly in the Appendix C PCB Layout Guidelines. Analyzing the EVB9S12XEP100 board, I found that 10uF polarized capacitors are used together with the decoupling capacitors, however, I did not find reference to these 10uF capacitors in the MC9S12XEP100 datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) The VDPLL, VDD, VDDF pins have 220nF decoupling capacitors to earth, however. Since the EVB9S12XEP100 evaluation board makes them available externally, I would like to know if there is a need to connect these pins to an external voltage source .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) Regarding the ocylator circuit, I noticed that, on the EVB9S12XEP100 card, there are two circuits, one of them uses full swing Pierce (FSP) with crystal and the other uses a clock generator. Is there any reason to use the external clock instead of a higher frequency oscillator?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With my best regards,&lt;/P&gt;&lt;P&gt;Daniel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2020 18:43:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Prototype-using-MC9S12XEP100-based-on-VB9S12XEP100/m-p/1039934#M4479</guid>
      <dc:creator>danielflor</dc:creator>
      <dc:date>2020-05-18T18:43:18Z</dc:date>
    </item>
    <item>
      <title>Re: Prototype using MC9S12XEP100 based on VB9S12XEP100</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Prototype-using-MC9S12XEP100-based-on-VB9S12XEP100/m-p/1039935#M4480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&lt;BR /&gt;You can refer to this application note:&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN3262.pdf"&gt;AN3262 Designing Hardware for the MC9S12X D-Family&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107388iD54AB24C9FD35FDA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2.&lt;BR /&gt;No, these are outputs not inputs of the internal voltage regulator.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107543i60EAB112E888C2F1/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107427i4460C5310423C7D3/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.&lt;/P&gt;&lt;P&gt;It is an addition option, if you need to use an external oscillator for some reasons.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 May 2020 11:03:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Prototype-using-MC9S12XEP100-based-on-VB9S12XEP100/m-p/1039935#M4480</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-05-19T11:03:01Z</dc:date>
    </item>
    <item>
      <title>Re: Prototype using MC9S12XEP100 based on VB9S12XEP100</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Prototype-using-MC9S12XEP100-based-on-VB9S12XEP100/m-p/1039936#M4481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you, Daniel, This document AN3262 will be very useful. But I still have another doubt, on the EVB9S12XEP100, there is a inductor of 10uH between VDD and VDDA, I guess it is there to remove high frequency components of the digital circuitry and separate them of the analog circuitry, but I didn't find any mention about it on the related documents.&lt;/P&gt;&lt;P&gt;So, I would like to know if is mandatory to have this inductor or in which cases it is recommended.&lt;/P&gt;&lt;P&gt;With my best regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2020 14:30:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Prototype-using-MC9S12XEP100-based-on-VB9S12XEP100/m-p/1039936#M4481</guid>
      <dc:creator>danielflor</dc:creator>
      <dc:date>2020-05-20T14:30:16Z</dc:date>
    </item>
    <item>
      <title>Re: Prototype using MC9S12XEP100 based on VB9S12XEP100</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Prototype-using-MC9S12XEP100-based-on-VB9S12XEP100/m-p/1039937#M4482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Daniel,&lt;/P&gt;&lt;P&gt;Yes, it can help to decouple the analog circuit but this is not required.&lt;/P&gt;&lt;P&gt;It was discussed, for example, here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/300771"&gt;ACD Reference Voltages&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/476060"&gt;https://community.nxp.com/thread/476060&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 May 2020 12:37:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Prototype-using-MC9S12XEP100-based-on-VB9S12XEP100/m-p/1039937#M4482</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-05-21T12:37:05Z</dc:date>
    </item>
  </channel>
</rss>