<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Cannot use PE TSI component with S08PT60 in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Cannot-use-PE-TSI-component-with-S08PT60/m-p/178258#M431</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the enlightment. I have checked on the TSS Suite. I just wonder if it only comprises the "software enabled" version for most microcontrollers, or if it takes into account the hardware TSI module of S08PT series.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Jul 2012 07:57:19 GMT</pubDate>
    <dc:creator>quevedo</dc:creator>
    <dc:date>2012-07-10T07:57:19Z</dc:date>
    <item>
      <title>Cannot use PE TSI component with S08PT60</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Cannot-use-PE-TSI-component-with-S08PT60/m-p/178256#M429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to write an application for the demo board TWR-208DC-PT60, which features a S08PT60VLH microcontroller. This board has one touch electrode, connected to one of the TSI-enabled pins of the controller. I have made all updates to Processor Expert, and also loaded the service packs for all S08Px series. However, when I try to use PE TSI component, the Component inspector tells me that this device has not TSI capability.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What could be going wrong?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jul 2012 23:58:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Cannot-use-PE-TSI-component-with-S08PT60/m-p/178256#M429</guid>
      <dc:creator>quevedo</dc:creator>
      <dc:date>2012-07-06T23:58:23Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot use PE TSI component with S08PT60</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Cannot-use-PE-TSI-component-with-S08PT60/m-p/178257#M430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;in case you want only initialization code it should be possible to use Init_TSI component, in case you want additional sw layer you should use TSS_Library component.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However the TSS_Library component is not delivered within the product by default and it must be additionaly downloaded from web.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/tss" rel="nofollow" target="_blank"&gt;www.freescale.com/tss&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Vojtech Filip&lt;BR /&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jul 2012 14:21:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Cannot-use-PE-TSI-component-with-S08PT60/m-p/178257#M430</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2012-07-09T14:21:01Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot use PE TSI component with S08PT60</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Cannot-use-PE-TSI-component-with-S08PT60/m-p/178258#M431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the enlightment. I have checked on the TSS Suite. I just wonder if it only comprises the "software enabled" version for most microcontrollers, or if it takes into account the hardware TSI module of S08PT series.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jul 2012 07:57:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Cannot-use-PE-TSI-component-with-S08PT60/m-p/178258#M431</guid>
      <dc:creator>quevedo</dc:creator>
      <dc:date>2012-07-10T07:57:19Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot use PE TSI component with S08PT60</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Cannot-use-PE-TSI-component-with-S08PT60/m-p/178259#M432</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;on PT family is encapsulated hardware TSI module, on the former S08, where was not TSI module, TSS can work with KBI, GPIO, FTM, TPM...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Vojtech Filip&lt;BR /&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jul 2012 13:34:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Cannot-use-PE-TSI-component-with-S08PT60/m-p/178259#M432</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2012-07-10T13:34:14Z</dc:date>
    </item>
  </channel>
</rss>