<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックI can not use the DDR2 driver with the Processor Expert</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/I-can-not-use-the-DDR2-driver-with-the-Processor-Expert/m-p/694917#M4063</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;Hi, I have the Code Warrior for MCU V10.6.4 Build: 150416 &lt;BR /&gt; I create a new project to use the DDR2 memory of the TWR-K70F120M board, I am trying to configure it with the Prosessor Expert but I do not get it to work. The configuration of the DDR2 driver extract them from appendix B of the document entitled "Relocating Code and Data Using the CW GCC Linker File (.ld) for Kinetis". When I attempt to enter debug mode an error appears and after several tests I find that the error occurs when writing to DDR_CR00, but also happens if I write to any DDR_CRXX. &lt;BR /&gt; Attached I send some images in Images.zip file: &lt;BR /&gt; Image 1: Code Warrior ready to enter debug. &lt;BR /&gt; Image 2: When it enters the debug mode, it is already in trouble because it can not initialize. &lt;BR /&gt; Image 3: after resetting I can enter debug mode before initialization. &lt;BR /&gt; Image 4: I click on "Run to this line" and until then it works well. &lt;BR /&gt; Image 5: When I click on "Run to this line" on the next line I lose the communication. &lt;BR /&gt; Image 6: When I try to pause the debug, the error appears. &lt;BR /&gt; I've been working on this for two weeks and I have to give it an end. Also try to copy the code in appendix B of the document already named but obtained the same result. &lt;BR /&gt; I enclose the complete project (K70_LCD.zip)&lt;BR /&gt; &lt;BR /&gt;&lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338778"&gt;Images.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338778"&gt;K70_LCD.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Aug 2017 17:39:56 GMT</pubDate>
    <dc:creator>diegoperea</dc:creator>
    <dc:date>2017-08-09T17:39:56Z</dc:date>
    <item>
      <title>I can not use the DDR2 driver with the Processor Expert</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/I-can-not-use-the-DDR2-driver-with-the-Processor-Expert/m-p/694917#M4063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;Hi, I have the Code Warrior for MCU V10.6.4 Build: 150416 &lt;BR /&gt; I create a new project to use the DDR2 memory of the TWR-K70F120M board, I am trying to configure it with the Prosessor Expert but I do not get it to work. The configuration of the DDR2 driver extract them from appendix B of the document entitled "Relocating Code and Data Using the CW GCC Linker File (.ld) for Kinetis". When I attempt to enter debug mode an error appears and after several tests I find that the error occurs when writing to DDR_CR00, but also happens if I write to any DDR_CRXX. &lt;BR /&gt; Attached I send some images in Images.zip file: &lt;BR /&gt; Image 1: Code Warrior ready to enter debug. &lt;BR /&gt; Image 2: When it enters the debug mode, it is already in trouble because it can not initialize. &lt;BR /&gt; Image 3: after resetting I can enter debug mode before initialization. &lt;BR /&gt; Image 4: I click on "Run to this line" and until then it works well. &lt;BR /&gt; Image 5: When I click on "Run to this line" on the next line I lose the communication. &lt;BR /&gt; Image 6: When I try to pause the debug, the error appears. &lt;BR /&gt; I've been working on this for two weeks and I have to give it an end. Also try to copy the code in appendix B of the document already named but obtained the same result. &lt;BR /&gt; I enclose the complete project (K70_LCD.zip)&lt;BR /&gt; &lt;BR /&gt;&lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338778"&gt;Images.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338778"&gt;K70_LCD.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Aug 2017 17:39:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/I-can-not-use-the-DDR2-driver-with-the-Processor-Expert/m-p/694917#M4063</guid>
      <dc:creator>diegoperea</dc:creator>
      <dc:date>2017-08-09T17:39:56Z</dc:date>
    </item>
    <item>
      <title>Re: I can not use the DDR2 driver with the Processor Expert</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/I-can-not-use-the-DDR2-driver-with-the-Processor-Expert/m-p/694918#M4064</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&amp;nbsp;Thanks to NXP support, you can solve the problem. Basically the PLL1 was incorrectly configured in the Expert Processor and the initialization was done according to the document "Relocating Code and Data Using the CW GCC Linker File (.ld) for Kinetis". It is important to clarify that the MK70FN1M0.mem file must be modified according to appendix D of the document. Attached the project in operation.&lt;BR /&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Diego Perea&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Aug 2017 03:04:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/I-can-not-use-the-DDR2-driver-with-the-Processor-Expert/m-p/694918#M4064</guid>
      <dc:creator>diegoperea</dc:creator>
      <dc:date>2017-08-11T03:04:05Z</dc:date>
    </item>
  </channel>
</rss>