<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: Using serial at the FRDM-25Z board</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Using-serial-at-the-FRDM-25Z-board/m-p/671173#M4021</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marcos,&lt;/P&gt;&lt;P&gt;- Please first be sure the UART port is right .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- The component of "CosnsoleIO" can used to send data through UART:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19746i30C4D246C5E32A86/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;- If still can't use , please tell me which IDE and which version do you used ? &lt;/P&gt;&lt;P&gt;And also send your project to me , or I don't know where is the "FSL_DEBUG_CONSOLE functions"&lt;/P&gt;&lt;P&gt;and "dbg_putchar() ".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Jun 2017 06:39:28 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2017-06-05T06:39:28Z</dc:date>
    <item>
      <title>Using serial at the FRDM-25Z board</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Using-serial-at-the-FRDM-25Z-board/m-p/671172#M4020</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to communicate with my FRDM-25Z board, using the FSL_DEBUG_CONSOLE functions and RTOS. But, I can't find the port configuration to initiate the service.The dbg_init() function doesn't work. Seems to me that I need create the pins configuration to this work. I used the 0u pin to receive data (RX) and 1u to transmit (TX) . the software has no errors, but nothing appears at the serial port, when i use the dbg_putchar() command. I'm using a serial monitor at PC to spy the data, and the baud rate is defined at 115200. &amp;nbsp;Someone has the configuration code to use this?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Jun 2017 13:45:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Using-serial-at-the-FRDM-25Z-board/m-p/671172#M4020</guid>
      <dc:creator>marcosgalelli</dc:creator>
      <dc:date>2017-06-01T13:45:33Z</dc:date>
    </item>
    <item>
      <title>Re: Using serial at the FRDM-25Z board</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Using-serial-at-the-FRDM-25Z-board/m-p/671173#M4021</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marcos,&lt;/P&gt;&lt;P&gt;- Please first be sure the UART port is right .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- The component of "CosnsoleIO" can used to send data through UART:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19746i30C4D246C5E32A86/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;- If still can't use , please tell me which IDE and which version do you used ? &lt;/P&gt;&lt;P&gt;And also send your project to me , or I don't know where is the "FSL_DEBUG_CONSOLE functions"&lt;/P&gt;&lt;P&gt;and "dbg_putchar() ".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jun 2017 06:39:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Using-serial-at-the-FRDM-25Z-board/m-p/671173#M4021</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-06-05T06:39:28Z</dc:date>
    </item>
  </channel>
</rss>