<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 Re: TimerUnit_LDD - SelectInputFrequency Method</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/TimerUnit-LDD-SelectInputFrequency-Method/m-p/662070#M4002</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;You can disable the generating of the code for your whole project by using the Processor Expert properties (Properties of the project) by settings the &lt;EM&gt;Disable Processor Expert changes &lt;/EM&gt;to &lt;EM&gt;yes. &lt;/EM&gt;See the following screenshot:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4131i25816AF8889F2C3A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition, you can also disable generating code for each component by using the &lt;EM&gt;Code Generation&lt;/EM&gt; option in the context menu of the component (in the &lt;EM&gt;Components&lt;/EM&gt; window), see the following screenshot:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_5.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4162iEE8D54F814672BE0/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Jan 2017 10:30:47 GMT</pubDate>
    <dc:creator>marek_neuzil</dc:creator>
    <dc:date>2017-01-02T10:30:47Z</dc:date>
    <item>
      <title>TimerUnit_LDD - SelectInputFrequency Method</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/TimerUnit-LDD-SelectInputFrequency-Method/m-p/662069#M4001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;TimerUnit_LDD - SelectInputFrequency Method&lt;/P&gt;&lt;P&gt;Processor Expert seems to decide for itself when to generate or not generate this code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For this component, I have Input Clock Source set to "Internal" and I have two different frequencies listed in the dialog box. I am using Advanced visibility.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the Component Inspector Methods tab, most methods let me choose "don't generate code" or "generate code" for each method. However for SelectInputFrequency (and a couple other methods) this option is grayed out. Sometimes "don't generate code" is selected and I can't change it. Other times "generate code" is selected and I can't change it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I really want to do is generate the code once so I can see what's going on, then not generate code for production.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~LMG&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 18:45:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/TimerUnit-LDD-SelectInputFrequency-Method/m-p/662069#M4001</guid>
      <dc:creator>lmg</dc:creator>
      <dc:date>2016-12-09T18:45:49Z</dc:date>
    </item>
    <item>
      <title>Re: TimerUnit_LDD - SelectInputFrequency Method</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/TimerUnit-LDD-SelectInputFrequency-Method/m-p/662070#M4002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;You can disable the generating of the code for your whole project by using the Processor Expert properties (Properties of the project) by settings the &lt;EM&gt;Disable Processor Expert changes &lt;/EM&gt;to &lt;EM&gt;yes. &lt;/EM&gt;See the following screenshot:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4131i25816AF8889F2C3A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition, you can also disable generating code for each component by using the &lt;EM&gt;Code Generation&lt;/EM&gt; option in the context menu of the component (in the &lt;EM&gt;Components&lt;/EM&gt; window), see the following screenshot:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_5.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4162iEE8D54F814672BE0/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Jan 2017 10:30:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/TimerUnit-LDD-SelectInputFrequency-Method/m-p/662070#M4002</guid>
      <dc:creator>marek_neuzil</dc:creator>
      <dc:date>2017-01-02T10:30:47Z</dc:date>
    </item>
  </channel>
</rss>