<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem using IntFLASH with 9S08 in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Problem-using-IntFLASH-with-9S08/m-p/659077#M3996</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anyone have an example using the Processor Expert IntFLASH bean with a 9S08 microcontroller? &amp;nbsp;I have been trying to use it with a MC9S08MM32A and have a strange problem. &amp;nbsp;I am able to write to flash, and verify the memory has changed (in debug), but when I power down and back up, my microcontroller hangs. &amp;nbsp;I have a timer interrupt that blinks an LED once per second and it never blinks after the first write and reboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I allocated my section of flash at 0xE000 with a size of 0x1000 &amp;nbsp;by reducing the size of the ROM section at 0xC000 to 0x2000. &amp;nbsp;I have also found that I can call the&amp;nbsp;IFsh1_EraseSector() function and&amp;nbsp;IFsh1_GetByteFlash() function without a problem, but if I call&amp;nbsp;IFsh1_SetByteFlash() it will cause the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This happens just by changing a single byte at 0xE100 from 0xFF to 0x00, &amp;nbsp;I can't see any other bytes in memory that have changed from my one function call.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Oct 2016 14:29:11 GMT</pubDate>
    <dc:creator>Spikey_Mikey</dc:creator>
    <dc:date>2016-10-21T14:29:11Z</dc:date>
    <item>
      <title>Problem using IntFLASH with 9S08</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Problem-using-IntFLASH-with-9S08/m-p/659077#M3996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anyone have an example using the Processor Expert IntFLASH bean with a 9S08 microcontroller? &amp;nbsp;I have been trying to use it with a MC9S08MM32A and have a strange problem. &amp;nbsp;I am able to write to flash, and verify the memory has changed (in debug), but when I power down and back up, my microcontroller hangs. &amp;nbsp;I have a timer interrupt that blinks an LED once per second and it never blinks after the first write and reboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I allocated my section of flash at 0xE000 with a size of 0x1000 &amp;nbsp;by reducing the size of the ROM section at 0xC000 to 0x2000. &amp;nbsp;I have also found that I can call the&amp;nbsp;IFsh1_EraseSector() function and&amp;nbsp;IFsh1_GetByteFlash() function without a problem, but if I call&amp;nbsp;IFsh1_SetByteFlash() it will cause the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This happens just by changing a single byte at 0xE100 from 0xFF to 0x00, &amp;nbsp;I can't see any other bytes in memory that have changed from my one function call.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Oct 2016 14:29:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Problem-using-IntFLASH-with-9S08/m-p/659077#M3996</guid>
      <dc:creator>Spikey_Mikey</dc:creator>
      <dc:date>2016-10-21T14:29:11Z</dc:date>
    </item>
    <item>
      <title>Re: Problem using IntFLASH with 9S08</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Problem-using-IntFLASH-with-9S08/m-p/659078#M3997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you use classic CW, You can check demo code under your CW install&lt;/P&gt;&lt;P&gt;{CW6.3 install}\ProcessorExpert\Projects\Test projects\IntFlash&lt;/P&gt;&lt;P&gt;more processor expert demo code&lt;/P&gt;&lt;P&gt;{CW6.3 install}\ProcessorExpert\Projects\Test projects&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can it help you?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Oct 2016 06:01:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Problem-using-IntFLASH-with-9S08/m-p/659078#M3997</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-10-24T06:01:54Z</dc:date>
    </item>
  </channel>
</rss>