<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックPE ADC &amp;quot;High&amp;quot; Level Component Problem for 56F827xx</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/PE-ADC-quot-High-quot-Level-Component-Problem-for-56F827xx/m-p/621249#M3963</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;I am setting up a PE ADC High level component and am having a problem with the Internal Trigger, Trigger Input settings.&amp;nbsp; This is for a 56F82748 DSC and using the 12 Bit Cyclic ADC.&lt;/P&gt;&lt;P&gt;I get the following error in the setttings.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14013i014491DC8C411F85/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and in the Problems it shows the following Errors.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14051i7456A6463BC0585B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The strange thing is that the ADC_LDD driver that the ADC High level component uses is happy...&lt;/P&gt;&lt;P&gt;&lt;IMG class="image-3 jive-image" src="https://community.nxp.com/" /&gt;&lt;/P&gt;&lt;P&gt;... and it is set to the same TA0_OUT.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14225i42EDDFFBDC00FFB7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The error message seems to indicate that the XBAR is not set up properly.&amp;nbsp; So I added it and the "Automatic" settings show that the timer I am using is routed to the ADC.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14187i2107EAFED9BCDE96/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;To me this seems like a bug but maybe I missed something.&lt;/P&gt;&lt;P&gt;Thanks for your Help!&lt;/P&gt;&lt;P&gt;Pete&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Feb 2017 18:10:35 GMT</pubDate>
    <dc:creator>dynapb</dc:creator>
    <dc:date>2017-02-09T18:10:35Z</dc:date>
    <item>
      <title>PE ADC "High" Level Component Problem for 56F827xx</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/PE-ADC-quot-High-quot-Level-Component-Problem-for-56F827xx/m-p/621249#M3963</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;I am setting up a PE ADC High level component and am having a problem with the Internal Trigger, Trigger Input settings.&amp;nbsp; This is for a 56F82748 DSC and using the 12 Bit Cyclic ADC.&lt;/P&gt;&lt;P&gt;I get the following error in the setttings.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14013i014491DC8C411F85/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and in the Problems it shows the following Errors.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14051i7456A6463BC0585B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The strange thing is that the ADC_LDD driver that the ADC High level component uses is happy...&lt;/P&gt;&lt;P&gt;&lt;IMG class="image-3 jive-image" src="https://community.nxp.com/" /&gt;&lt;/P&gt;&lt;P&gt;... and it is set to the same TA0_OUT.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14225i42EDDFFBDC00FFB7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The error message seems to indicate that the XBAR is not set up properly.&amp;nbsp; So I added it and the "Automatic" settings show that the timer I am using is routed to the ADC.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14187i2107EAFED9BCDE96/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;To me this seems like a bug but maybe I missed something.&lt;/P&gt;&lt;P&gt;Thanks for your Help!&lt;/P&gt;&lt;P&gt;Pete&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Feb 2017 18:10:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/PE-ADC-quot-High-quot-Level-Component-Problem-for-56F827xx/m-p/621249#M3963</guid>
      <dc:creator>dynapb</dc:creator>
      <dc:date>2017-02-09T18:10:35Z</dc:date>
    </item>
  </channel>
</rss>