<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic commonreginitialization.prg problems in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/commonreginitialization-prg-problems/m-p/613170#M3957</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear anyone who read this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found a bug in PE:&lt;/P&gt;&lt;P&gt;When you add a Init_UART in you project, here my chip is KL02z32, It seems that you can't setting the interrupt of the uart to 1-3, or you will get an error when you generate PE code.&lt;/P&gt;&lt;P&gt;the error is as following:&lt;/P&gt;&lt;P&gt;Description Resource Path Location Type&lt;BR /&gt;Generator: FAILURE: Unexpected status of script: Drivers\Common\CommonRegInitialization.prg, please contact Freescale support. R485Repeator Cpu Processor Expert Problem&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the setting 0 works well.&lt;/P&gt;&lt;P&gt;anyway, I have not checked on the datasheet, maybe the interrupt of uart is limited on int0...maybe I will study the datasheet a few hours later and I will update in the following posts if there are any needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for reading and anything for all~ and hope there are fixes for this issue( or this bug.)&lt;/P&gt;&lt;P&gt;BR.&lt;/P&gt;&lt;P&gt;/Zona&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Dec 2016 14:58:53 GMT</pubDate>
    <dc:creator>zhaowum</dc:creator>
    <dc:date>2016-12-14T14:58:53Z</dc:date>
    <item>
      <title>commonreginitialization.prg problems</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/commonreginitialization-prg-problems/m-p/613170#M3957</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear anyone who read this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found a bug in PE:&lt;/P&gt;&lt;P&gt;When you add a Init_UART in you project, here my chip is KL02z32, It seems that you can't setting the interrupt of the uart to 1-3, or you will get an error when you generate PE code.&lt;/P&gt;&lt;P&gt;the error is as following:&lt;/P&gt;&lt;P&gt;Description Resource Path Location Type&lt;BR /&gt;Generator: FAILURE: Unexpected status of script: Drivers\Common\CommonRegInitialization.prg, please contact Freescale support. R485Repeator Cpu Processor Expert Problem&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the setting 0 works well.&lt;/P&gt;&lt;P&gt;anyway, I have not checked on the datasheet, maybe the interrupt of uart is limited on int0...maybe I will study the datasheet a few hours later and I will update in the following posts if there are any needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for reading and anything for all~ and hope there are fixes for this issue( or this bug.)&lt;/P&gt;&lt;P&gt;BR.&lt;/P&gt;&lt;P&gt;/Zona&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 14:58:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/commonreginitialization-prg-problems/m-p/613170#M3957</guid>
      <dc:creator>zhaowum</dc:creator>
      <dc:date>2016-12-14T14:58:53Z</dc:date>
    </item>
    <item>
      <title>Re: commonreginitialization.prg problems</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/commonreginitialization-prg-problems/m-p/613171#M3958</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have read the datasheet MKE02P064M40SFORM.PDF, and it is in the page52. It said that the NVIC IPR rigister number of the UARTx is 3, is it means fixed in 3?&lt;/P&gt;&lt;P&gt;But why in KDS3.2, the pe only can work when the interrupt level set in 0?&lt;/P&gt;&lt;P&gt;Anyone can help to make me clear?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for reading.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Zona&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 02:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/commonreginitialization-prg-problems/m-p/613171#M3958</guid>
      <dc:creator>zhaowum</dc:creator>
      <dc:date>2016-12-15T02:26:48Z</dc:date>
    </item>
  </channel>
</rss>