<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Cpu_SetFlexNVMPartition() function fails in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Cpu-SetFlexNVMPartition-function-fails/m-p/584364#M3931</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The issue has been already discussed, see the discussion thread &lt;A href="https://community.nxp.com/thread/383738"&gt;Return ERR_FAILED when calling Cpu_SetFlexNVMPartition() using KDS, PE and K10&lt;/A&gt; &lt;/P&gt;&lt;P&gt;You can also find a demo application, see the discussion thread &lt;A href="https://community.nxp.com/thread/336949"&gt;Reset when calling SetFlexNVMPartition() using KDS, PE and K22&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Jul 2016 06:25:55 GMT</pubDate>
    <dc:creator>marek_neuzil</dc:creator>
    <dc:date>2016-07-04T06:25:55Z</dc:date>
    <item>
      <title>Cpu_SetFlexNVMPartition() function fails</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Cpu-SetFlexNVMPartition-function-fails/m-p/584363#M3930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the Kinetis MK20DX256VLQ10 with CodeWarrior 10.6.4 with all current updates.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Processor Expert is configured for 512 bytes of EEPROM, 50/50 split and all 256K for EEPROM backup (0x2506).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to partition this correctly when downloading with CodeWarrior and PROGACMP using a MultiLink Universal FX.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried putting a call to Cpu_SetFlexRAMFunction( FlexRAM_AS_EEPROM ) prior to calling Cpu_SetFlexNVMPartition() to insure that the FlexRAM is set for EEPROM and that function fails also.&amp;nbsp; Both with the Access Error flag set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have single stepped the machine language and it looks like everything is setup appropriately.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have researched this on the forums and haven't found an answer.&amp;nbsp; This is not a stack overflow problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have seen this work on single step and i am trying to recreate the successful procedure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jun 2016 18:26:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Cpu-SetFlexNVMPartition-function-fails/m-p/584363#M3930</guid>
      <dc:creator>mikekatz</dc:creator>
      <dc:date>2016-06-28T18:26:06Z</dc:date>
    </item>
    <item>
      <title>Re: Cpu_SetFlexNVMPartition() function fails</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Cpu-SetFlexNVMPartition-function-fails/m-p/584364#M3931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The issue has been already discussed, see the discussion thread &lt;A href="https://community.nxp.com/thread/383738"&gt;Return ERR_FAILED when calling Cpu_SetFlexNVMPartition() using KDS, PE and K10&lt;/A&gt; &lt;/P&gt;&lt;P&gt;You can also find a demo application, see the discussion thread &lt;A href="https://community.nxp.com/thread/336949"&gt;Reset when calling SetFlexNVMPartition() using KDS, PE and K22&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jul 2016 06:25:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Cpu-SetFlexNVMPartition-function-fails/m-p/584364#M3931</guid>
      <dc:creator>marek_neuzil</dc:creator>
      <dc:date>2016-07-04T06:25:55Z</dc:date>
    </item>
  </channel>
</rss>