<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 Why doesn't PE generate #include for header</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Why-doesn-t-PE-generate-include-for-header/m-p/508968#M3907</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a KDS 3.1 project using Processor Expert 1.12.2.RT7_b1550-0615 with KSDK 1.2. Recently I added the HWTIMER component and it generated a hwTim1.c and hwTim1.h. However, the hwTim1.c file did not contain the #include "hwTim1.h" preprocessor line so the build fails and I have to add that line manually. So, of course, every time PE syncs it overwrites that line and I have to fix it repeatedly. My other components do not have this issue. Is there a way to fix this or is this a problem with this specific component?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Mar 2016 22:03:36 GMT</pubDate>
    <dc:creator>ericnetherland</dc:creator>
    <dc:date>2016-03-28T22:03:36Z</dc:date>
    <item>
      <title>Why doesn't PE generate #include for header</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Why-doesn-t-PE-generate-include-for-header/m-p/508968#M3907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a KDS 3.1 project using Processor Expert 1.12.2.RT7_b1550-0615 with KSDK 1.2. Recently I added the HWTIMER component and it generated a hwTim1.c and hwTim1.h. However, the hwTim1.c file did not contain the #include "hwTim1.h" preprocessor line so the build fails and I have to add that line manually. So, of course, every time PE syncs it overwrites that line and I have to fix it repeatedly. My other components do not have this issue. Is there a way to fix this or is this a problem with this specific component?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Mar 2016 22:03:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Why-doesn-t-PE-generate-include-for-header/m-p/508968#M3907</guid>
      <dc:creator>ericnetherland</dc:creator>
      <dc:date>2016-03-28T22:03:36Z</dc:date>
    </item>
    <item>
      <title>Re: Why doesn't PE generate #include for header</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Why-doesn-t-PE-generate-include-for-header/m-p/508969#M3908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can work-around this by disabling code generation of this component. To use this feature just right click on the component and select "Dont Write..." command in "Code Generation" menu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26223i2ADF9BF40625C789/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Vojtech Filip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Mar 2016 10:19:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Why-doesn-t-PE-generate-include-for-header/m-p/508969#M3908</guid>
      <dc:creator>vfilip</dc:creator>
      <dc:date>2016-03-29T10:19:54Z</dc:date>
    </item>
    <item>
      <title>Re: Why doesn't PE generate #include for header</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Why-doesn-t-PE-generate-include-for-header/m-p/508970#M3909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Thank you for reporting of this issue. The issue can be reproduced when the Callback property is set to Disabled and the Kinetis SDK 1.2.0 is used. In this case, use the workaround that has been published by Vojtech Filip, please.&lt;/P&gt;&lt;P&gt;Please note that the fsl_hwtimer component has been already fixed in the Processor Expert for KSDK 1.3.0 version (KSDK 1.3.0 Eclipse Update).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Mar 2016 12:01:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Why-doesn-t-PE-generate-include-for-header/m-p/508970#M3909</guid>
      <dc:creator>marek_neuzil</dc:creator>
      <dc:date>2016-03-29T12:01:52Z</dc:date>
    </item>
  </channel>
</rss>