<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Processor Expert TimerOut_LDD in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-TimerOut-LDD/m-p/488127#M3812</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in TimerUnit_LDD, you can change the period of the whole timer using SetPeriodTicks method and also compare value for individual channels using SetOffsetTicks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PPG_LDD can change period or frequency (SetFrequencykHz etc...) during runtime. see attached video for PPG component usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Jan 2016 04:53:02 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2016-01-14T04:53:02Z</dc:date>
    <item>
      <title>Processor Expert TimerOut_LDD</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-TimerOut-LDD/m-p/488126#M3811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to put out a pulse width at 50% duty cycle.&amp;nbsp; The frequency can be between 500Hz and 5KHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using a MKL36Z128VLL4 and another board uses the MKL36Z256Vll4 chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I right click on 'TimerOut_LDD' select 'Add to Project' and select the 'New component[TimerUnit_LDD]...'&lt;/P&gt;&lt;P&gt;Compare is TPM1_C1V, pin is LCD_P60/ADC0_DM0/ADC0_SE4a/PTE21/TPM1_CH1/UART0_RX.&amp;nbsp; I then select the Pulse Width but the 'Runtime setting type is 'Fixed Value' no other option is available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to have a range of frequency (pulse outputs as stated above).&amp;nbsp; How can I get the Processor Expert system give me what I need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the first time that I have used Code Warrior and Processor Expert so a detailed step to follow to achieve my goal would be great.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;John Vogel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2016 12:16:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-TimerOut-LDD/m-p/488126#M3811</guid>
      <dc:creator>haroldvogel</dc:creator>
      <dc:date>2016-01-13T12:16:38Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert TimerOut_LDD</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-TimerOut-LDD/m-p/488127#M3812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in TimerUnit_LDD, you can change the period of the whole timer using SetPeriodTicks method and also compare value for individual channels using SetOffsetTicks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PPG_LDD can change period or frequency (SetFrequencykHz etc...) during runtime. see attached video for PPG component usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jan 2016 04:53:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-TimerOut-LDD/m-p/488127#M3812</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-01-14T04:53:02Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert TimerOut_LDD</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-TimerOut-LDD/m-p/488128#M3813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SetPeriodTicks is not in the list of items.  Here is the list the bold items I can select:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yours truly,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;John Vogel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jan 2016 11:53:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-TimerOut-LDD/m-p/488128#M3813</guid>
      <dc:creator>haroldvogel</dc:creator>
      <dc:date>2016-01-14T11:53:36Z</dc:date>
    </item>
  </channel>
</rss>