<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: Clocking the MK20FX512 with Processor Expert?</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Clocking-the-MK20FX512-with-Processor-Expert/m-p/486932#M3804</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Simon Haines:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let us know the version of Processor Expert or the IDE version that you are using (Codewarrior or Kinetis Design Studio).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you sure you selected K20FX512 from the New Project Wizard?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This device does not have any &lt;STRONG&gt;RTC_CLKIN&lt;/STRONG&gt; pin, only the &lt;STRONG&gt;XTAL32/EXTAL32&lt;/STRONG&gt; pins for the crystal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using KDS v3.1.0 I do not have any issues to set your required configuration, see below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56049i490D7EEFACA7312B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Jan 2016 18:03:41 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2016-01-25T18:03:41Z</dc:date>
    <item>
      <title>Clocking the MK20FX512 with Processor Expert?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Clocking-the-MK20FX512-with-Processor-Expert/m-p/486931#M3803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to clock a Kinetis MK20FX512 at 96MHz core clock speed and 48MHz bus speed with Processor Expert. I have a 32.768kHz crystal attached to XTAL32/EXTAL32 (with nothing on XTAL0/EXTAL0 and XTAL1/EXTAL1) and I am able to set the following configuration manually in code:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;RTC OSCE 32.768 kHz oscillator is enabled&lt;/LI&gt;&lt;LI&gt;SIM OSC32KSEL RTC oscillator selected as 32kHz clock source (ERCLK32K)&lt;/LI&gt;&lt;LI&gt;SIM PLLFLLSEL MCGFLLCLK selected for various peripheral clocking options&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="line-height: 1.5;"&gt;SIM OUTDIV1 Sys: /1&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;SIM OUTDIV2 Bus: /2&lt;/LI&gt;&lt;LI&gt;OSC0 ERCLKEN External reference clock enabled&lt;/LI&gt;&lt;LI&gt;OSC1 ERCLKEN External reference clock enabled&lt;/LI&gt;&lt;LI&gt;MCG OSCSEL 32kHz RTC oscillator selected as FLL external reference clock&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="line-height: 1.5;"&gt;MCG RANGE0 Low frequency range selected for crystal oscillator&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;MCG HGO0 High gain oscillator configured for low-power operation&lt;/LI&gt;&lt;LI&gt;MCG EREFS0 External reference clock selected (not oscillator) as EREF source&lt;/LI&gt;&lt;LI&gt;MCG IRCS Slow internal reference clock selected (instead of fast IREF)&lt;/LI&gt;&lt;LI&gt;MCG CLKS Output of FLL selected as clock source&lt;/LI&gt;&lt;LI&gt;MCG FRDIV /1 divider for external reference clock (OSCSEL has reset value of 0)&lt;/LI&gt;&lt;LI&gt;MCG IREFS External reference clock selected as source for the FLL&lt;/LI&gt;&lt;LI&gt;MCG IRCLKEN Internal reference clock is enabled&lt;/LI&gt;&lt;LI&gt;MCG IREFSTEN Internal reference clock is disabled in stop mode&lt;/LI&gt;&lt;LI&gt;MCG DMX32 DRST_DRS DCO range is 96MHz&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This produces the desired core clock speed of 96MHz and bus speed of 48MHz. Using processor expert, I can't select XTAL32/EXTAL32 as the clock source for the RTC (only RTC_CLKIN is available) or the DMX32 and DRST_DRS values to get the clock to 96MHz. The highest value seems to be 47.972352MHz. Is this a problem with my configuration or with Processor Expert?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2016 04:23:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Clocking-the-MK20FX512-with-Processor-Expert/m-p/486931#M3803</guid>
      <dc:creator>simonhaines</dc:creator>
      <dc:date>2016-01-13T04:23:12Z</dc:date>
    </item>
    <item>
      <title>Re: Clocking the MK20FX512 with Processor Expert?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Clocking-the-MK20FX512-with-Processor-Expert/m-p/486932#M3804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Simon Haines:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let us know the version of Processor Expert or the IDE version that you are using (Codewarrior or Kinetis Design Studio).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you sure you selected K20FX512 from the New Project Wizard?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This device does not have any &lt;STRONG&gt;RTC_CLKIN&lt;/STRONG&gt; pin, only the &lt;STRONG&gt;XTAL32/EXTAL32&lt;/STRONG&gt; pins for the crystal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using KDS v3.1.0 I do not have any issues to set your required configuration, see below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56049i490D7EEFACA7312B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jan 2016 18:03:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Clocking-the-MK20FX512-with-Processor-Expert/m-p/486932#M3804</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2016-01-25T18:03:41Z</dc:date>
    </item>
    <item>
      <title>Re: Clocking the MK20FX512 with Processor Expert?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Clocking-the-MK20FX512-with-Processor-Expert/m-p/486933#M3805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jorge, double-checking my setup shows I had indeed selected the wrong chip (off by one error ha ha). Thanks for taking the time to reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jan 2016 22:54:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Clocking-the-MK20FX512-with-Processor-Expert/m-p/486933#M3805</guid>
      <dc:creator>simonhaines</dc:creator>
      <dc:date>2016-01-25T22:54:48Z</dc:date>
    </item>
  </channel>
</rss>