<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックAdding Processor Expert to a KSDK example project</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Adding-Processor-Expert-to-a-KSDK-example-project/m-p/470737#M3749</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the KSDK 1.3.0 USB host keyboard example running on a FRDM-K22F. The example that I chose is using FreeRTOS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used the KSDK Project Generator to clone the keyboard example from:&lt;/P&gt;&lt;P&gt;C:\Freescale\KSDK_1.3.0\examples\frdmk22f\demo_apps\usb\host\hid\keyboard&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My next task is to port this example to our custom board which uses an MK22FN512VMP12 and then add some additional functionality.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to use Processor Expert with this project and I'm wondering which is the best way to do this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;* Create a new project with KSDK and Processor Expert and then pull in the necessary files from the USB host keyboard example?&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;* Add Processor Expert to the existing cloned project? Per something like this:&amp;nbsp; &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-102365"&gt;https://community.freescale.com/docs/DOC-102365&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using:&lt;/P&gt;&lt;P&gt;* KDS 3.0 with the 3.1 update&lt;/P&gt;&lt;P&gt;* KSDK 1.3.0&lt;/P&gt;&lt;P&gt;* FreeRTOS&lt;/P&gt;&lt;P&gt;* KSDK Project Generator 2.0&lt;/P&gt;&lt;P&gt;* FRDM-K22F&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone offer guidance on this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Allen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Feb 2016 20:42:36 GMT</pubDate>
    <dc:creator>gorakk</dc:creator>
    <dc:date>2016-02-19T20:42:36Z</dc:date>
    <item>
      <title>Adding Processor Expert to a KSDK example project</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Adding-Processor-Expert-to-a-KSDK-example-project/m-p/470737#M3749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the KSDK 1.3.0 USB host keyboard example running on a FRDM-K22F. The example that I chose is using FreeRTOS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used the KSDK Project Generator to clone the keyboard example from:&lt;/P&gt;&lt;P&gt;C:\Freescale\KSDK_1.3.0\examples\frdmk22f\demo_apps\usb\host\hid\keyboard&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My next task is to port this example to our custom board which uses an MK22FN512VMP12 and then add some additional functionality.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to use Processor Expert with this project and I'm wondering which is the best way to do this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;* Create a new project with KSDK and Processor Expert and then pull in the necessary files from the USB host keyboard example?&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;* Add Processor Expert to the existing cloned project? Per something like this:&amp;nbsp; &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-102365"&gt;https://community.freescale.com/docs/DOC-102365&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using:&lt;/P&gt;&lt;P&gt;* KDS 3.0 with the 3.1 update&lt;/P&gt;&lt;P&gt;* KSDK 1.3.0&lt;/P&gt;&lt;P&gt;* FreeRTOS&lt;/P&gt;&lt;P&gt;* KSDK Project Generator 2.0&lt;/P&gt;&lt;P&gt;* FRDM-K22F&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone offer guidance on this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Allen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Feb 2016 20:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Adding-Processor-Expert-to-a-KSDK-example-project/m-p/470737#M3749</guid>
      <dc:creator>gorakk</dc:creator>
      <dc:date>2016-02-19T20:42:36Z</dc:date>
    </item>
    <item>
      <title>Re: Adding Processor Expert to a KSDK example project</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Adding-Processor-Expert-to-a-KSDK-example-project/m-p/470738#M3750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Allen,&lt;/P&gt;&lt;P&gt;regarding to your two options, I think option 1 is easier to handle the project.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Feb 2016 02:51:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Adding-Processor-Expert-to-a-KSDK-example-project/m-p/470738#M3750</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-02-23T02:51:54Z</dc:date>
    </item>
  </channel>
</rss>