<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Wakeup from VLLS3 using TSI configures through Processor Expert? in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Wakeup-from-VLLS3-using-TSI-configures-through-Processor-Expert/m-p/470249#M3747</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on a small message panel using a Kinetis KL05 device. I want it to stay in a low-power mode, keeping the message to be displayed in RAM. Thus, I decided to enter VLLS3 mode. I want to wake up the device using a TSI electrode, and I have configured the PE TSS_Library component to use PTA9 as the wakeup electrode. CPU component is configured to FEI clock mode (default). I can use the Cpu_SetOperationMode() function to put the device into VLLS3, but my TSI electrode does not wake it up.&lt;/P&gt;&lt;P&gt;I am not using a FRDM board, it is a custom board, with an external USBDM debugger. There is an LED connected (cathode) to pin PTB1. The test project (CW10.6) is attached to this question.&lt;/P&gt;&lt;P&gt;I know that there are some examples for low-power wakeup, but I would prefer a step-by-step description of how can I program the device for working as described above. For example, if I have to configure RTC to hardware trigger the TSI, if I can use the LPO source for RTC, and so on.&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Antonio&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-339184"&gt;TestVLLS.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 12 Mar 2016 18:30:25 GMT</pubDate>
    <dc:creator>quevedo</dc:creator>
    <dc:date>2016-03-12T18:30:25Z</dc:date>
    <item>
      <title>Wakeup from VLLS3 using TSI configures through Processor Expert?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Wakeup-from-VLLS3-using-TSI-configures-through-Processor-Expert/m-p/470249#M3747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on a small message panel using a Kinetis KL05 device. I want it to stay in a low-power mode, keeping the message to be displayed in RAM. Thus, I decided to enter VLLS3 mode. I want to wake up the device using a TSI electrode, and I have configured the PE TSS_Library component to use PTA9 as the wakeup electrode. CPU component is configured to FEI clock mode (default). I can use the Cpu_SetOperationMode() function to put the device into VLLS3, but my TSI electrode does not wake it up.&lt;/P&gt;&lt;P&gt;I am not using a FRDM board, it is a custom board, with an external USBDM debugger. There is an LED connected (cathode) to pin PTB1. The test project (CW10.6) is attached to this question.&lt;/P&gt;&lt;P&gt;I know that there are some examples for low-power wakeup, but I would prefer a step-by-step description of how can I program the device for working as described above. For example, if I have to configure RTC to hardware trigger the TSI, if I can use the LPO source for RTC, and so on.&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Antonio&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-339184"&gt;TestVLLS.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Mar 2016 18:30:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Wakeup-from-VLLS3-using-TSI-configures-through-Processor-Expert/m-p/470249#M3747</guid>
      <dc:creator>quevedo</dc:creator>
      <dc:date>2016-03-12T18:30:25Z</dc:date>
    </item>
    <item>
      <title>Re: Wakeup from VLLS3 using TSI configures through Processor Expert?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Wakeup-from-VLLS3-using-TSI-configures-through-Processor-Expert/m-p/470250#M3748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Antonio,&lt;/P&gt;&lt;P&gt;The TSS_Library component is provided by a Sensor team (they have developed the library and the Processor Expert Component). You can post your question on the Sensor community (&lt;A href="https://community.nxp.com/space/11146"&gt;Sensors&lt;/A&gt; ) if you need details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have checked your application and I see following issue:&lt;/P&gt;&lt;P&gt;The &lt;EM&gt;TSS Config Register Init\System Configuration Register\LowPower Enabled&lt;/EM&gt; must be set to &lt;EM&gt;yes&lt;/EM&gt;. See below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="TSS_library_low_power.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56467i6B53EE4B19173BC0/image-size/large?v=v2&amp;amp;px=999" role="button" title="TSS_library_low_power.png" alt="TSS_library_low_power.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The TSI functionality in the VLLS3 power mode is restricted, see the description in the reference manual:&lt;/P&gt;&lt;P&gt; &lt;SPAN style="font-size: 9.0pt; font-family: 'HelveticaLTStd-Roman',sans-serif;"&gt;TSI module is fully functional in all of the stop modes as long&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt; font-family: 'HelveticaLTStd-Roman',sans-serif;"&gt;as TSI_GENCS[STPE] is set. The channel specified by&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt; font-family: 'HelveticaLTStd-Roman',sans-serif;"&gt;TSI_DATA[TSICH] will be scanned upon the trigger. After&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt; font-family: 'HelveticaLTStd-Roman',sans-serif;"&gt;scan finishes, either end-of-scan or out-of-range interrupt can&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt; font-family: 'HelveticaLTStd-Roman',sans-serif;"&gt;be selected to bring MCU out of low power modes.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You must also configure the LLWU device and enabled TSI0 as the wake-up source.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Apr 2016 08:58:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Wakeup-from-VLLS3-using-TSI-configures-through-Processor-Expert/m-p/470250#M3748</guid>
      <dc:creator>marek_neuzil</dc:creator>
      <dc:date>2016-04-29T08:58:48Z</dc:date>
    </item>
  </channel>
</rss>