<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックCAN_LDD</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/CAN-LDD/m-p/467419#M3743</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to get a CAN_LDD interface working on a MK60FX512 and I am noticing that the SYNCH bit in ESR1 of the Flexcan module is set, meaning that the "FlexCAN is not synchronized to the CAN bus."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can only assume that this is why when I send data from the micro to another device, that the data doesn't come across.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the "Sending data frame with interrupt service" example provided in the documentation and the CAN1_OnFreeTxBuffer is never hit on a break point.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, is it correct that I would be seeing pulses on the CAN bus if I am not actively sending data?&amp;nbsp; I don't recall from the standard if there is continual packets for timing being transmitted.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Feb 2016 21:31:18 GMT</pubDate>
    <dc:creator>markbishop</dc:creator>
    <dc:date>2016-02-17T21:31:18Z</dc:date>
    <item>
      <title>CAN_LDD</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/CAN-LDD/m-p/467419#M3743</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to get a CAN_LDD interface working on a MK60FX512 and I am noticing that the SYNCH bit in ESR1 of the Flexcan module is set, meaning that the "FlexCAN is not synchronized to the CAN bus."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can only assume that this is why when I send data from the micro to another device, that the data doesn't come across.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the "Sending data frame with interrupt service" example provided in the documentation and the CAN1_OnFreeTxBuffer is never hit on a break point.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, is it correct that I would be seeing pulses on the CAN bus if I am not actively sending data?&amp;nbsp; I don't recall from the standard if there is continual packets for timing being transmitted.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Feb 2016 21:31:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/CAN-LDD/m-p/467419#M3743</guid>
      <dc:creator>markbishop</dc:creator>
      <dc:date>2016-02-17T21:31:18Z</dc:date>
    </item>
    <item>
      <title>Re: CAN_LDD</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/CAN-LDD/m-p/467420#M3744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-&amp;nbsp; "the SYNCH bit in ESR1 of the Flexcan module is set", this meaning FlexCAN is synchronized to the CAN bus.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53838i544DC5D14F347A4E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;- And &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53906i036BCCAC7E1364D5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt; , could you please tell me which DOC ?&lt;/P&gt;&lt;P&gt;And also do you meaning when you test the example you mentioned , it can not work well ? If yes,&lt;/P&gt;&lt;P&gt;please tell me which , i can check on my side .&lt;/P&gt;&lt;P&gt;You can also describe your problem in detail .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Feb 2016 06:40:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/CAN-LDD/m-p/467420#M3744</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-02-19T06:40:45Z</dc:date>
    </item>
  </channel>
</rss>