<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 Using TPMxCLK</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Using-TPMxCLK/m-p/456814#M3699</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could someone please explain to me how I can set up the MC9S08QE32 to use an external clock ref (TPMxCLK) on any of the timer modules, in PE. How do specify which pin is the input clk? How do I specify the xCLK frequency?&lt;/P&gt;&lt;P&gt;I am using Freescale Codewarrior 5.9.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Sep 2015 22:49:28 GMT</pubDate>
    <dc:creator>mahkamehvarza</dc:creator>
    <dc:date>2015-09-16T22:49:28Z</dc:date>
    <item>
      <title>Using TPMxCLK</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Using-TPMxCLK/m-p/456814#M3699</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could someone please explain to me how I can set up the MC9S08QE32 to use an external clock ref (TPMxCLK) on any of the timer modules, in PE. How do specify which pin is the input clk? How do I specify the xCLK frequency?&lt;/P&gt;&lt;P&gt;I am using Freescale Codewarrior 5.9.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Sep 2015 22:49:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Using-TPMxCLK/m-p/456814#M3699</guid>
      <dc:creator>mahkamehvarza</dc:creator>
      <dc:date>2015-09-16T22:49:28Z</dc:date>
    </item>
    <item>
      <title>Re: Using TPMxCLK</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Using-TPMxCLK/m-p/456815#M3700</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use CW10.6 , i can configure the external clock source of TPM as this :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52218i94398FF09C297B18/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And please&amp;nbsp; screenshot your CW, and does it have the same view ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Sep 2015 02:31:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Using-TPMxCLK/m-p/456815#M3700</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-09-21T02:31:42Z</dc:date>
    </item>
  </channel>
</rss>