<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 Re: MSCAN S08DZ Reciecver Interrupt Problem</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/MSCAN-S08DZ-Reciecver-Interrupt-Problem/m-p/173605#M365</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is an example project. I expect it to toogle a LED everytime a CAN message is sent.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Jun 2012 21:54:08 GMT</pubDate>
    <dc:creator>Swood</dc:creator>
    <dc:date>2012-06-22T21:54:08Z</dc:date>
    <item>
      <title>MSCAN S08DZ Reciecver Interrupt Problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/MSCAN-S08DZ-Reciecver-Interrupt-Problem/m-p/173602#M362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;First off, I'm using CW 5.9.0 with PE 3.07.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've done all the obvious code changes for the CAN, but I cannot get it to generate an interrupt on receiver full. The Rx Acceptance ID masks are set to al FFs, and the Acceptance Mode is set to Two 32bit Filters. I've looked at the clock and bit rate settings and they look right for 500Kbit/s operation, but I cannot get the system to generate an interrupt. The interrupt service just toggles an LED right now. It looks like the CAN_Init function is being called the CANE bit is being set.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What else should I be looking at to get this running?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Stuart&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jun 2012 19:58:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/MSCAN-S08DZ-Reciecver-Interrupt-Problem/m-p/173602#M362</guid>
      <dc:creator>Swood</dc:creator>
      <dc:date>2012-06-20T19:58:22Z</dc:date>
    </item>
    <item>
      <title>Re: MSCAN S08DZ Reciecver Interrupt Problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/MSCAN-S08DZ-Reciecver-Interrupt-Problem/m-p/173603#M363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you please post a sample zipped project showing the problem or screenshots of all your component settings?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Petr Hradsky&lt;BR /&gt;Processor Expert Support and Servicepacks Team&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jun 2012 17:16:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/MSCAN-S08DZ-Reciecver-Interrupt-Problem/m-p/173603#M363</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2012-06-21T17:16:33Z</dc:date>
    </item>
    <item>
      <title>Re: MSCAN S08DZ Reciecver Interrupt Problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/MSCAN-S08DZ-Reciecver-Interrupt-Problem/m-p/173604#M364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does this Help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jun 2012 02:23:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/MSCAN-S08DZ-Reciecver-Interrupt-Problem/m-p/173604#M364</guid>
      <dc:creator>Swood</dc:creator>
      <dc:date>2012-06-22T02:23:24Z</dc:date>
    </item>
    <item>
      <title>Re: MSCAN S08DZ Reciecver Interrupt Problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/MSCAN-S08DZ-Reciecver-Interrupt-Problem/m-p/173605#M365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is an example project. I expect it to toogle a LED everytime a CAN message is sent.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jun 2012 21:54:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/MSCAN-S08DZ-Reciecver-Interrupt-Problem/m-p/173605#M365</guid>
      <dc:creator>Swood</dc:creator>
      <dc:date>2012-06-22T21:54:08Z</dc:date>
    </item>
    <item>
      <title>Re: MSCAN S08DZ Reciecver Interrupt Problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/MSCAN-S08DZ-Reciecver-Interrupt-Problem/m-p/173606#M366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;From a &amp;nbsp;look on the project, I don't see anything that would be clearly wrong... However, t&lt;SPAN&gt;here might be some timing setup or other issue.&amp;nbsp;&lt;/SPAN&gt;I recommend to enable the Error interupt and create a simple handler for it and check if any error occurs by putting breakpoint inside.&lt;/P&gt;&lt;P&gt;Do you have a properly configured &amp;nbsp;board? It might be also useful to check with scope if there is actuall some signal on the selected CAN pins of the MCU.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Petr Hradsky&lt;BR /&gt;Processor Expert Support Team&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2012 20:53:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/MSCAN-S08DZ-Reciecver-Interrupt-Problem/m-p/173606#M366</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2012-06-26T20:53:09Z</dc:date>
    </item>
    <item>
      <title>Re: MSCAN S08DZ Receiver Interrupt Problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/MSCAN-S08DZ-Reciecver-Interrupt-Problem/m-p/173607#M367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've added the Error Interrupts and it is going into the Error Passive state due to receive errors.&lt;/P&gt;&lt;P&gt;There is data on the bus. I've attached scope captures of the working HC08GZ and the NOT working HCS08DZ. A Grid Connect USB/CAN Adaptor transmits data from a test program.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2012 00:46:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/MSCAN-S08DZ-Reciecver-Interrupt-Problem/m-p/173607#M367</guid>
      <dc:creator>Swood</dc:creator>
      <dc:date>2012-06-27T00:46:51Z</dc:date>
    </item>
  </channel>
</rss>